<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックA71CH ConstructedSecret Question</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/A71CH-ConstructedSecret-Question/m-p/1379983#M622</link>
    <description>&lt;P&gt;Section 6.2.2.1 "ConstructedSecret" of AN12229 "APDU Specification of A71CH Security Module Rev. 3.0" describes a method for creating longer secrets from the 8 available 128bit symmetric keys available in the part.&amp;nbsp; It indicates that the Constructed Secret is formed from two nibbles of a byte where the upper nibble is the number of 128bit symmetric keys to be used and the lower nibble is the starting index.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If we choose the lower nibble to be 0x7 meaning symmetric key #8 and we select the upper nibble to be 0x3 meaning three 128bit keys, would the keys wrap so that they are #8, #1, &amp;amp; #2?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Dec 2021 18:23:41 GMT</pubDate>
    <dc:creator>michael_d_adams</dc:creator>
    <dc:date>2021-12-01T18:23:41Z</dc:date>
    <item>
      <title>A71CH ConstructedSecret Question</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A71CH-ConstructedSecret-Question/m-p/1379983#M622</link>
      <description>&lt;P&gt;Section 6.2.2.1 "ConstructedSecret" of AN12229 "APDU Specification of A71CH Security Module Rev. 3.0" describes a method for creating longer secrets from the 8 available 128bit symmetric keys available in the part.&amp;nbsp; It indicates that the Constructed Secret is formed from two nibbles of a byte where the upper nibble is the number of 128bit symmetric keys to be used and the lower nibble is the starting index.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If we choose the lower nibble to be 0x7 meaning symmetric key #8 and we select the upper nibble to be 0x3 meaning three 128bit keys, would the keys wrap so that they are #8, #1, &amp;amp; #2?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Dec 2021 18:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A71CH-ConstructedSecret-Question/m-p/1379983#M622</guid>
      <dc:creator>michael_d_adams</dc:creator>
      <dc:date>2021-12-01T18:23:41Z</dc:date>
    </item>
    <item>
      <title>Re: A71CH ConstructedSecret Question</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A71CH-ConstructedSecret-Question/m-p/1380312#M623</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/134782"&gt;@michael_d_adams&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No, such kind of wrap feature is not supported.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 02 Dec 2021 06:20:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A71CH-ConstructedSecret-Question/m-p/1380312#M623</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-12-02T06:20:40Z</dc:date>
    </item>
  </channel>
</rss>