<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックSE050 ed25519 (EdDSA) example code</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-ed25519-EdDSA-example-code/m-p/1314661#M552</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any available example code that deals with EdDSA? I am unable to find much in reference to this in the documentation or examples.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ethan&lt;/P&gt;</description>
    <pubDate>Wed, 28 Jul 2021 16:12:38 GMT</pubDate>
    <dc:creator>ethanlooney</dc:creator>
    <dc:date>2021-07-28T16:12:38Z</dc:date>
    <item>
      <title>SE050 ed25519 (EdDSA) example code</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-ed25519-EdDSA-example-code/m-p/1314661#M552</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any available example code that deals with EdDSA? I am unable to find much in reference to this in the documentation or examples.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ethan&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 16:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-ed25519-EdDSA-example-code/m-p/1314661#M552</guid>
      <dc:creator>ethanlooney</dc:creator>
      <dc:date>2021-07-28T16:12:38Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 ed25519 (EdDSA) example code</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-ed25519-EdDSA-example-code/m-p/1318628#M557</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186080"&gt;@ethanlooney&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no example available for EdDSA, but the best demo&amp;nbsp;as base for EdDSA is ex_ecc. Please kindly refer to the attachment for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 05 Aug 2021 02:59:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-ed25519-EdDSA-example-code/m-p/1318628#M557</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-08-05T02:59:12Z</dc:date>
    </item>
  </channel>
</rss>