<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure Authentication中的主题 porting SE050 driver to U-Boot</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/porting-SE050-driver-to-U-Boot/m-p/1314313#M551</link>
    <description>&lt;P&gt;Hello community,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;We are planning to use SE050 in our design to do signature verification of the Linux kernel at U-Boot stage as part of the secure boot process.&lt;/P&gt;&lt;P&gt;Is there any official port of SE050 driver to U-Boot? mainline and/or vendor U-Boot?&lt;BR /&gt;If yes, where can I find it?&lt;BR /&gt;If not, what would be the process to port it? are there some guidelines specifically for porting to U-Boot?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support!&lt;BR /&gt;Best regards,&lt;/P&gt;&lt;P&gt;A_1359&lt;/P&gt;</description>
    <pubDate>Wed, 28 Jul 2021 06:54:40 GMT</pubDate>
    <dc:creator>a_1359</dc:creator>
    <dc:date>2021-07-28T06:54:40Z</dc:date>
    <item>
      <title>porting SE050 driver to U-Boot</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/porting-SE050-driver-to-U-Boot/m-p/1314313#M551</link>
      <description>&lt;P&gt;Hello community,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;We are planning to use SE050 in our design to do signature verification of the Linux kernel at U-Boot stage as part of the secure boot process.&lt;/P&gt;&lt;P&gt;Is there any official port of SE050 driver to U-Boot? mainline and/or vendor U-Boot?&lt;BR /&gt;If yes, where can I find it?&lt;BR /&gt;If not, what would be the process to port it? are there some guidelines specifically for porting to U-Boot?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support!&lt;BR /&gt;Best regards,&lt;/P&gt;&lt;P&gt;A_1359&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 06:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/porting-SE050-driver-to-U-Boot/m-p/1314313#M551</guid>
      <dc:creator>a_1359</dc:creator>
      <dc:date>2021-07-28T06:54:40Z</dc:date>
    </item>
    <item>
      <title>Re: porting SE050 driver to U-Boot</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/porting-SE050-driver-to-U-Boot/m-p/1315108#M553</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/154211"&gt;@a_1359&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For U-Boot, we have no SE05x integration, but we provide an app note for that topic. Please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12448.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12448.pdf&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 08:05:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/porting-SE050-driver-to-U-Boot/m-p/1315108#M553</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-07-29T08:05:28Z</dc:date>
    </item>
  </channel>
</rss>