<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic determine if Platform SCP keys are correct in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/determine-if-Platform-SCP-keys-are-correct/m-p/1306343#M537</link>
    <description>&lt;P&gt;I'm using the middleware 3.0.6 and implemented the Patform SCP key rotation example for a SE050C2. This works as desired but when I later try to connect again with the (no longer valid) default keys without selecting the applet "&lt;EM&gt;sss_session_open()&lt;/EM&gt;" returns success and only later commands fail.&lt;/P&gt;&lt;P&gt;"&lt;EM&gt;nxScp03_HostLocal_VerifyCardCryptogram()&lt;/EM&gt;"&amp;nbsp;and&amp;nbsp;"&lt;EM&gt;AuthenticateChannel()&lt;/EM&gt;" both&amp;nbsp;return fail but "&lt;EM&gt;sss_session_open()&lt;/EM&gt;" does not propagate this failure and only a log message "Could not set SCP03 Secure Channel" is output.&lt;/P&gt;&lt;P&gt;Shouldn't&amp;nbsp;"&lt;EM&gt;sss_session_open()&lt;/EM&gt;" fail if the Platform SCP keys provided are wrong?&lt;/P&gt;</description>
    <pubDate>Mon, 12 Jul 2021 20:07:04 GMT</pubDate>
    <dc:creator>fus</dc:creator>
    <dc:date>2021-07-12T20:07:04Z</dc:date>
    <item>
      <title>determine if Platform SCP keys are correct</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/determine-if-Platform-SCP-keys-are-correct/m-p/1306343#M537</link>
      <description>&lt;P&gt;I'm using the middleware 3.0.6 and implemented the Patform SCP key rotation example for a SE050C2. This works as desired but when I later try to connect again with the (no longer valid) default keys without selecting the applet "&lt;EM&gt;sss_session_open()&lt;/EM&gt;" returns success and only later commands fail.&lt;/P&gt;&lt;P&gt;"&lt;EM&gt;nxScp03_HostLocal_VerifyCardCryptogram()&lt;/EM&gt;"&amp;nbsp;and&amp;nbsp;"&lt;EM&gt;AuthenticateChannel()&lt;/EM&gt;" both&amp;nbsp;return fail but "&lt;EM&gt;sss_session_open()&lt;/EM&gt;" does not propagate this failure and only a log message "Could not set SCP03 Secure Channel" is output.&lt;/P&gt;&lt;P&gt;Shouldn't&amp;nbsp;"&lt;EM&gt;sss_session_open()&lt;/EM&gt;" fail if the Platform SCP keys provided are wrong?&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jul 2021 20:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/determine-if-Platform-SCP-keys-are-correct/m-p/1306343#M537</guid>
      <dc:creator>fus</dc:creator>
      <dc:date>2021-07-12T20:07:04Z</dc:date>
    </item>
    <item>
      <title>Re: determine if Platform SCP keys are correct</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/determine-if-Platform-SCP-keys-are-correct/m-p/1312268#M545</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/149297"&gt;@fus&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the report! Our MW team has confirmed this and will fix it in&amp;nbsp;&lt;SPAN&gt;future MW versions.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jul 2021 01:47:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/determine-if-Platform-SCP-keys-are-correct/m-p/1312268#M545</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-07-23T01:47:22Z</dc:date>
    </item>
  </channel>
</rss>