<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックSE050 change default I2C address</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-change-default-I2C-address/m-p/1269078#M484</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;The default slave address of the SE050 is configured to 0x48. How it can be changed?&lt;BR /&gt;Regards, Tomek&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 27 Apr 2021 17:20:23 GMT</pubDate>
    <dc:creator>atc024</dc:creator>
    <dc:date>2021-04-27T17:20:23Z</dc:date>
    <item>
      <title>SE050 change default I2C address</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-change-default-I2C-address/m-p/1269078#M484</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;The default slave address of the SE050 is configured to 0x48. How it can be changed?&lt;BR /&gt;Regards, Tomek&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 17:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-change-default-I2C-address/m-p/1269078#M484</guid>
      <dc:creator>atc024</dc:creator>
      <dc:date>2021-04-27T17:20:23Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 change default I2C address</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-change-default-I2C-address/m-p/1269514#M486</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186128"&gt;@atc024&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No, SE050 doesn't support this, but it is possible with SE051, please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13015" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=AN13015&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 08:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-change-default-I2C-address/m-p/1269514#M486</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-04-28T08:37:02Z</dc:date>
    </item>
  </channel>
</rss>