<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Use plug &amp;amp; trust library for a71ch in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Use-plug-amp-trust-library-for-a71ch/m-p/1243417#M472</link>
    <description>&lt;P&gt;I have a running application on a nrf52840 that generates a random number, generates a keypair, hashes, signs and verifies a signature over the sss API on the SE050. I now want to use the same application on the A71CH, is this possible? According to the&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=SE050-PLUG-TRUST-MW&amp;amp;location=null" target="_self"&gt;plug and trust MW documentation&lt;/A&gt;&amp;nbsp;those functions were all mapped from the a71ch host library to the sss api. Where is the mapping done in the library?&lt;/P&gt;&lt;P&gt;As far as i understood, I should be able to edit the&amp;nbsp; fsl_sss_ftr_default.h file in a way that it compiles the sss api for the a71ch. If this is correct, is there an example that shows how I am supposed to set the defines? I cant seem to figure out how, is there a documentation that describes the dependencies?&amp;nbsp;&lt;/P&gt;&lt;P&gt;E.g: When I choose SSS_HAVE_APPLET_A71CH (and no other applet) the define for the T1oI2C is set, which is only needed for the SE050.&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Lea&lt;/P&gt;</description>
    <pubDate>Wed, 10 Mar 2021 16:51:09 GMT</pubDate>
    <dc:creator>ziml</dc:creator>
    <dc:date>2021-03-10T16:51:09Z</dc:date>
    <item>
      <title>Use plug &amp; trust library for a71ch</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Use-plug-amp-trust-library-for-a71ch/m-p/1243417#M472</link>
      <description>&lt;P&gt;I have a running application on a nrf52840 that generates a random number, generates a keypair, hashes, signs and verifies a signature over the sss API on the SE050. I now want to use the same application on the A71CH, is this possible? According to the&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=SE050-PLUG-TRUST-MW&amp;amp;location=null" target="_self"&gt;plug and trust MW documentation&lt;/A&gt;&amp;nbsp;those functions were all mapped from the a71ch host library to the sss api. Where is the mapping done in the library?&lt;/P&gt;&lt;P&gt;As far as i understood, I should be able to edit the&amp;nbsp; fsl_sss_ftr_default.h file in a way that it compiles the sss api for the a71ch. If this is correct, is there an example that shows how I am supposed to set the defines? I cant seem to figure out how, is there a documentation that describes the dependencies?&amp;nbsp;&lt;/P&gt;&lt;P&gt;E.g: When I choose SSS_HAVE_APPLET_A71CH (and no other applet) the define for the T1oI2C is set, which is only needed for the SE050.&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Lea&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 16:51:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Use-plug-amp-trust-library-for-a71ch/m-p/1243417#M472</guid>
      <dc:creator>ziml</dc:creator>
      <dc:date>2021-03-10T16:51:09Z</dc:date>
    </item>
    <item>
      <title>Re: Use plug &amp; trust library for a71ch</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Use-plug-amp-trust-library-for-a71ch/m-p/1244705#M473</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/155870"&gt;@ziml&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The latest SE050 MW supports A71CH as well, you may refer to "SE-PLUG-TRUST-MW/simw-top/doc/a71ch/a71ch_miscellaneous.html#demos-and-examples-supported-on-a71ch" for more details regarding the changes made for testing with A71CH.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 12 Mar 2021 08:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Use-plug-amp-trust-library-for-a71ch/m-p/1244705#M473</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-03-12T08:55:13Z</dc:date>
    </item>
  </channel>
</rss>