<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Encrypt more than 128 Byte of source data Using AES 128 on SE050 in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Encrypt-more-than-128-Byte-of-source-data-Using-AES-128-on-SE050/m-p/1195149#M415</link>
    <description>&lt;P&gt;Hi Folks,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I am using the SE050 development board for encryption purposes and I was checking the ex_symmetric example given in Plug and trust middleware. The example is given as 128 bits of Key, input data, and IV.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do we encrypt if we have more than 128 bits of input data?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Aslam&lt;/P&gt;</description>
    <pubDate>Tue, 08 Dec 2020 05:19:17 GMT</pubDate>
    <dc:creator>mohamedaslam_m</dc:creator>
    <dc:date>2020-12-08T05:19:17Z</dc:date>
    <item>
      <title>Encrypt more than 128 Byte of source data Using AES 128 on SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Encrypt-more-than-128-Byte-of-source-data-Using-AES-128-on-SE050/m-p/1195149#M415</link>
      <description>&lt;P&gt;Hi Folks,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I am using the SE050 development board for encryption purposes and I was checking the ex_symmetric example given in Plug and trust middleware. The example is given as 128 bits of Key, input data, and IV.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do we encrypt if we have more than 128 bits of input data?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Aslam&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 05:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Encrypt-more-than-128-Byte-of-source-data-Using-AES-128-on-SE050/m-p/1195149#M415</guid>
      <dc:creator>mohamedaslam_m</dc:creator>
      <dc:date>2020-12-08T05:19:17Z</dc:date>
    </item>
    <item>
      <title>Re: Encrypt more than 128 Byte of source data Using AES 128 on SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Encrypt-more-than-128-Byte-of-source-data-Using-AES-128-on-SE050/m-p/1196168#M420</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/145386"&gt;@mohamedaslam_m&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The following functions are provided for your case, the basic steps are init-&amp;gt;update-&amp;gt;update ... -&amp;gt;finish, as described in AN12413.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sss functions for cipher operation.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/132216iBA51C46054782EBE/image-size/large?v=v2&amp;amp;px=999" role="button" title="sss functions for cipher operation.png" alt="sss functions for cipher operation.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;sss functions for cipher operation.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that makes sense,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 09 Dec 2020 08:29:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Encrypt-more-than-128-Byte-of-source-data-Using-AES-128-on-SE050/m-p/1196168#M420</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-12-09T08:29:28Z</dc:date>
    </item>
  </channel>
</rss>