<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: A71CH and TLS 1.3 in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/A71CH-and-TLS-1-3/m-p/855406#M35</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it supports. Actually &lt;SPAN style="font-size: 11.0pt;"&gt;limiting factor here is just the version of OpenSSL which we have in our PSP code. With the crypto capabilities of the A71CH also TLS 1.3 authentication have to be possible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Jan 2019 08:24:21 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2019-01-30T08:24:21Z</dc:date>
    <item>
      <title>A71CH and TLS 1.3</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A71CH-and-TLS-1-3/m-p/855405#M34</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;will the A71CH support TLS version 1.3 ? I can read that currently the chip support TLS 1.2.&lt;/P&gt;&lt;P&gt;More in general, can this chip be upgraded to follow new TLS releases once installed ?&lt;/P&gt;&lt;P&gt;Let's say, what&amp;nbsp;happens when a vulnerability is discovered on TLS 1.2 implementation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2019 14:21:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A71CH-and-TLS-1-3/m-p/855405#M34</guid>
      <dc:creator>antoniosantagiu</dc:creator>
      <dc:date>2019-01-23T14:21:50Z</dc:date>
    </item>
    <item>
      <title>Re: A71CH and TLS 1.3</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A71CH-and-TLS-1-3/m-p/855406#M35</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it supports. Actually &lt;SPAN style="font-size: 11.0pt;"&gt;limiting factor here is just the version of OpenSSL which we have in our PSP code. With the crypto capabilities of the A71CH also TLS 1.3 authentication have to be possible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 08:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A71CH-and-TLS-1-3/m-p/855406#M35</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-01-30T08:24:21Z</dc:date>
    </item>
  </channel>
</rss>