<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックIs it possible to program and add custom applets in EdgeLock SE050?</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-program-and-add-custom-applets-in-EdgeLock/m-p/1150346#M341</link>
    <description>&lt;P&gt;I would like to know if there are any possibilities of programming our own custom applets in EdgeLock SE050.&lt;/P&gt;&lt;P&gt;If Yes, Then It would be very helpful to know the procedure, If there is any, for installing custom applets in EdgeLock SE050.&lt;/P&gt;&lt;P&gt;Thank You.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 08 Sep 2020 11:50:10 GMT</pubDate>
    <dc:creator>Gauravraikar</dc:creator>
    <dc:date>2020-09-08T11:50:10Z</dc:date>
    <item>
      <title>Is it possible to program and add custom applets in EdgeLock SE050?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-program-and-add-custom-applets-in-EdgeLock/m-p/1150346#M341</link>
      <description>&lt;P&gt;I would like to know if there are any possibilities of programming our own custom applets in EdgeLock SE050.&lt;/P&gt;&lt;P&gt;If Yes, Then It would be very helpful to know the procedure, If there is any, for installing custom applets in EdgeLock SE050.&lt;/P&gt;&lt;P&gt;Thank You.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 11:50:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-program-and-add-custom-applets-in-EdgeLock/m-p/1150346#M341</guid>
      <dc:creator>Gauravraikar</dc:creator>
      <dc:date>2020-09-08T11:50:10Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to program and add custom applets in EdgeLock SE050?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-program-and-add-custom-applets-in-EdgeLock/m-p/1150875#M342</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Gauravraikar，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There has been threads on this topic, please kindly refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Secure-Authentication/Configurable-Modifiable-SE050-Product-Variants/m-p/1055778#M272" target="_blank"&gt;https://community.nxp.com/t5/Secure-Authentication/Configurable-Modifiable-SE050-Product-Variants/m-p/1055778#M272&lt;/A&gt; for details.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 06:45:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-program-and-add-custom-applets-in-EdgeLock/m-p/1150875#M342</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-09-09T06:45:37Z</dc:date>
    </item>
  </channel>
</rss>