<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: SE050ARD Antenna Design/Specification</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050ARD-Antenna-Design-Specification/m-p/1026260#M233</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also looking for the schematic and pcb design: EDA project or gerbers. I think that it is very important for antenna design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Julen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jun 2020 09:41:47 GMT</pubDate>
    <dc:creator>jgutierrez1</dc:creator>
    <dc:date>2020-06-19T09:41:47Z</dc:date>
    <item>
      <title>SE050ARD Antenna Design/Specification</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050ARD-Antenna-Design-Specification/m-p/1026258#M231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Regarding&amp;nbsp;AN12395OM-SE050ARD hardware overview the application schematic says, "Route Antenna as shown in reference design".&lt;/P&gt;&lt;P&gt;However the reference design is not included in the documents that can be downloaded from NxP's website. Where can I obtain the reference design or a specification for the antenna design?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2019 04:27:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050ARD-Antenna-Design-Specification/m-p/1026258#M231</guid>
      <dc:creator>davidward</dc:creator>
      <dc:date>2019-12-10T04:27:06Z</dc:date>
    </item>
    <item>
      <title>Re: SE050ARD Antenna Design/Specification</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050ARD-Antenna-Design-Specification/m-p/1026259#M232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the reference design in the AN might just mean the board, but anyway , what are you looking for indeed? Gerber File of OM-SE050ARD? Please kindly clarify. I may help to check if it is available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 09:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050ARD-Antenna-Design-Specification/m-p/1026259#M232</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-12-12T09:06:31Z</dc:date>
    </item>
    <item>
      <title>Re: SE050ARD Antenna Design/Specification</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050ARD-Antenna-Design-Specification/m-p/1026260#M233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also looking for the schematic and pcb design: EDA project or gerbers. I think that it is very important for antenna design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Julen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2020 09:41:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050ARD-Antenna-Design-Specification/m-p/1026260#M233</guid>
      <dc:creator>jgutierrez1</dc:creator>
      <dc:date>2020-06-19T09:41:47Z</dc:date>
    </item>
  </channel>
</rss>