<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to revert Platform SCP03 keys back to default using se05x_TP_PlatformSCP03keys.c? in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/How-to-revert-Platform-SCP03-keys-back-to-default-using-se05x-TP/m-p/2411213#M2148</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the clarification.&lt;/P&gt;&lt;P&gt;In my case, the current keys are known (0x4041... for ENC, MAC, and DEK), and I can successfully establish an SCP03 session using these keys via ssscli.&lt;/P&gt;&lt;P&gt;Since I have the current keys available to authenticate, could you please provide details on how to modify se05x_TP_PlatformSCP03keys.c to perform the key rotation back to the default values?&lt;/P&gt;&lt;P&gt;Specifically, I would like to know:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Which variables or macros should be updated with the current keys (0x4041...) for authentication during session setup.&lt;/LI&gt;&lt;LI&gt;Which variables or structures should hold the target default key values (ex_sss_tp_scp03_keys.h) for the PutKey operation.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any code snippets or specific line references in se05x_TP_PlatformSCP03keys.c (or related boot/auth headers) would be greatly appreciated.&lt;/P&gt;</description>
    <pubDate>Fri, 04 Sep 2026 07:36:37 GMT</pubDate>
    <dc:creator>Uc_S</dc:creator>
    <dc:date>2026-09-04T07:36:37Z</dc:date>
    <item>
      <title>How to revert Platform SCP03 keys back to default using se05x_TP_PlatformSCP03keys.c?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/How-to-revert-Platform-SCP03-keys-back-to-default-using-se05x-TP/m-p/2411142#M2146</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I am working with the SE051 secure element and would like to ask how to properly revert the Platform SCP03 keys back to their default values using the Plug and Trust Middleware.&lt;/P&gt;&lt;H4&gt;What I have done so far:&lt;/H4&gt;&lt;OL&gt;&lt;LI&gt;I modified demos/se05x/se05x_RotatePlatformSCP03Keys/se05x_TP_PlatformSCP03keys.c by commenting out the key reversion section (between doc:start:revert-scp03-keys and doc:end:revert-scp03-keys).&lt;/LI&gt;&lt;LI&gt;I built and executed the application on my setup.&lt;/LI&gt;&lt;LI&gt;The execution was successful, showing the message: "Congratulations !!! Key Rotation Successful!!!!"&lt;/LI&gt;&lt;LI&gt;To verify the key change, I updated /tmp/SE05X/plain_scp.txt with the new key value (0x4041... for ENC, MAC, and DEK) and successfully connected via ssscli connect.&lt;/LI&gt;&lt;LI&gt;Subsequent operations (ssscli generate rsa, ssscli set aes, and ssscli se05x readidlist) were all completed successfully, confirming that keys were written and IDs were retrieved without issues.&lt;/LI&gt;&lt;LI&gt;Now, I would like to restore the Platform SCP03 keys back to the default keys (defined in sss/ex/inc/ex_sss_tp_scp03_keys.h).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Could anyone guide me on how to modify se05x_TP_PlatformSCP03keys.c or what the correct process is to perform this key reversion?&lt;/P&gt;&lt;H4&gt;Environment:&lt;/H4&gt;&lt;UL&gt;&lt;LI&gt;Board: MCIMX8M-WEVK with OM-SE051ARD&lt;/LI&gt;&lt;LI&gt;Plug and Trust MW Version: v04.07.01&lt;/LI&gt;&lt;LI&gt;OP-TEE OS Version: 3.19.0&lt;/LI&gt;&lt;LI&gt;Linux Kernel: 6.1.151&lt;/LI&gt;&lt;LI&gt;OEF ID: A8FA&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any advice or code pointers would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Sep 2026 00:59:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/How-to-revert-Platform-SCP03-keys-back-to-default-using-se05x-TP/m-p/2411142#M2146</guid>
      <dc:creator>Uc_S</dc:creator>
      <dc:date>2026-09-04T00:59:57Z</dc:date>
    </item>
    <item>
      <title>Re: How to revert Platform SCP03 keys back to default using se05x_TP_PlatformSCP03keys.c?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/How-to-revert-Platform-SCP03-keys-back-to-default-using-se05x-TP/m-p/2411210#M2147</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259681"&gt;@Uc_S&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="p8i6j01 paragraph"&gt;Rotating the Platform SCP03 keys back to the default values is only possible when the &lt;STRONG&gt;current keys are known&lt;/STRONG&gt;, as a successfully authenticated SCP03 session is required before any key update (&lt;CODE class="p8i6j0f"&gt;PutKey&lt;/CODE&gt;) command can be issued to the SE051.&lt;/P&gt;
&lt;P class="p8i6j01 paragraph"&gt;If the current keys have been lost or forgotten, it is &lt;STRONG&gt;not possible&lt;/STRONG&gt; to authenticate to the SE051 and perform the key rotation. There is no backdoor or override mechanism — this is by design to preserve the security model of the device.&lt;/P&gt;
&lt;P class="p8i6j01 paragraph"&gt;Additionally, a factory reset does &lt;STRONG&gt;not&lt;/STRONG&gt; help, as Platform SCP03 keys are explicitly unaffected by the factory reset procedure. &lt;A id="base-ui-:r4ho:" class="wdbi343 wdbi341 _1ibi0s3ec _1ibi0s376" tabindex="0" role="button" href="https://nxp1-my.sharepoint.com/personal/kan_li_nxp_com/Documents/data%20sheet/SE051/doc/SE051%20-%20User%20Guidelines(AN12730.pdf?web=1" rel="noreferrer" aria-expanded="false" aria-haspopup="dialog" data-base-ui-click-trigger="" data-label="1" aria-label="Citation 1" target="_blank"&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P class="p8i6j01 paragraph"&gt;In this situation, the only option is to &lt;STRONG&gt;replace the SE051 with a new device&lt;/STRONG&gt; that still carries the default NXP-provisioned keys.&lt;/P&gt;
&lt;P class="p8i6j01 paragraph"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 04 Sep 2026 07:18:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/How-to-revert-Platform-SCP03-keys-back-to-default-using-se05x-TP/m-p/2411210#M2147</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2026-09-04T07:18:59Z</dc:date>
    </item>
    <item>
      <title>Re: How to revert Platform SCP03 keys back to default using se05x_TP_PlatformSCP03keys.c?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/How-to-revert-Platform-SCP03-keys-back-to-default-using-se05x-TP/m-p/2411213#M2148</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the clarification.&lt;/P&gt;&lt;P&gt;In my case, the current keys are known (0x4041... for ENC, MAC, and DEK), and I can successfully establish an SCP03 session using these keys via ssscli.&lt;/P&gt;&lt;P&gt;Since I have the current keys available to authenticate, could you please provide details on how to modify se05x_TP_PlatformSCP03keys.c to perform the key rotation back to the default values?&lt;/P&gt;&lt;P&gt;Specifically, I would like to know:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Which variables or macros should be updated with the current keys (0x4041...) for authentication during session setup.&lt;/LI&gt;&lt;LI&gt;Which variables or structures should hold the target default key values (ex_sss_tp_scp03_keys.h) for the PutKey operation.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any code snippets or specific line references in se05x_TP_PlatformSCP03keys.c (or related boot/auth headers) would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Sep 2026 07:36:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/How-to-revert-Platform-SCP03-keys-back-to-default-using-se05x-TP/m-p/2411213#M2148</guid>
      <dc:creator>Uc_S</dc:creator>
      <dc:date>2026-09-04T07:36:37Z</dc:date>
    </item>
    <item>
      <title>Re: How to revert Platform SCP03 keys back to default using se05x_TP_PlatformSCP03keys.c?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/How-to-revert-Platform-SCP03-keys-back-to-default-using-se05x-TP/m-p/2411228#M2150</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259681"&gt;@Uc_S&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;If you just need to rotate the keys back to the default,&amp;nbsp;the nano-package example is the &lt;STRONG&gt;recommended simpler path&lt;/STRONG&gt; — only the three &lt;CODE class="p8i6j0f"&gt;scp03_*&lt;/CODE&gt; arrays (current keys for auth) and the three &lt;CODE class="p8i6j0f"&gt;NEW_scp03_*&lt;/CODE&gt; arrays (default keys as target) need to be updated, and the revert call within&amp;nbsp;ex_se05x_rotate_scp03_keys() needs to be commented out. Please refer to the following for details.&lt;/P&gt;
&lt;H3 class="_9k2iva0 p8i6j0c _1ibi0s314 heading3 _9k2iva1"&gt;Change 1 — Set the current keys (used to open the SCP03 session)&lt;/H3&gt;
&lt;P class="p8i6j01 paragraph"&gt;Lines 38–43 are the auth keys passed to &lt;CODE class="p8i6j0f"&gt;ex_set_scp03_keys()&lt;/CODE&gt;. Replace the placeholder &lt;CODE class="p8i6j0f"&gt;0xABCD...&lt;/CODE&gt; values with your &lt;STRONG&gt;current keys&lt;/STRONG&gt; (&lt;CODE class="p8i6j0f"&gt;0x4041...&lt;/CODE&gt;&lt;LI-EMOJI id="lia_disappointed-face" title=":disappointed_face:"&gt;&lt;/LI-EMOJI&gt; &lt;A id="base-ui-:r4q5:" class="wdbi343 wdbi341 _1ibi0s3ec _1ibi0s376" tabindex="0" role="button" href="https://raw.githubusercontent.com/NXPPlugNTrust/nano-package/master/examples/se05x_rotate_scp03_keys/src/ex_se05x_rotate_scp03_keys.c" rel="noreferrer" aria-expanded="false" aria-haspopup="dialog" data-base-ui-click-trigger="" data-label="2" aria-label="Citation 2" target="_blank"&gt;&lt;/A&gt;&lt;/P&gt;
&lt;DIV class="l8rrz21 _1ibi0s3en" data-ui-element="code-block-container"&gt;
&lt;PRE&gt;&lt;CODE class="markdown-code-c p8i6j0e hljs language-c _12n1b832"&gt;&lt;SPAN class="hljs-type"&gt;uint8_t&lt;/SPAN&gt; scp03_enc_key[AES_KEY_LEN_nBYTE] = {
    &lt;SPAN class="hljs-number"&gt;0x40&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x41&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x42&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x43&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x44&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x45&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x46&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x47&lt;/SPAN&gt;,
    &lt;SPAN class="hljs-number"&gt;0x48&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x49&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4A&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4B&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4C&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4D&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4E&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4F&lt;/SPAN&gt; };

&lt;SPAN class="hljs-type"&gt;uint8_t&lt;/SPAN&gt; scp03_mac_key[AES_KEY_LEN_nBYTE] = {
    &lt;SPAN class="hljs-number"&gt;0x40&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x41&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x42&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x43&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x44&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x45&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x46&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x47&lt;/SPAN&gt;,
    &lt;SPAN class="hljs-number"&gt;0x48&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x49&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4A&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4B&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4C&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4D&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4E&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4F&lt;/SPAN&gt; };

&lt;SPAN class="hljs-type"&gt;uint8_t&lt;/SPAN&gt; scp03_dek_key[AES_KEY_LEN_nBYTE] = {
    &lt;SPAN class="hljs-number"&gt;0x40&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x41&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x42&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x43&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x44&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x45&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x46&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x47&lt;/SPAN&gt;,
    &lt;SPAN class="hljs-number"&gt;0x48&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x49&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4A&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4B&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4C&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4D&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4E&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x4F&lt;/SPAN&gt; };
&lt;/CODE&gt;&lt;/PRE&gt;
&lt;DIV class="l8rrz23 _1ibi0s3dp _1ibi0s332 _1ibi0s3eo _1ibi0s3bm _1ibi0s3ce"&gt;
&lt;DIV class="l8rrz25 _1ibi0s3eb"&gt;c&lt;/DIV&gt;
&lt;DIV class="lqznwq0"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;H3 class="_9k2iva0 p8i6j0c _1ibi0s314 heading3 _9k2iva1"&gt;Change 2 — Set the NEW target keys (the default SE051C A8FA keys)&lt;/H3&gt;
&lt;P class="p8i6j01 paragraph"&gt;Lines 45–50 are the keys that will be &lt;STRONG&gt;written into the SE051&lt;/STRONG&gt; via &lt;CODE class="p8i6j0f"&gt;PutKey&lt;/CODE&gt;. Replace the &lt;CODE class="p8i6j0f"&gt;0x4041...&lt;/CODE&gt; placeholder with the SE051C OEF A8FA default values: &lt;A id="base-ui-:r4qa:" class="wdbi343 wdbi341 _1ibi0s3ec _1ibi0s376" tabindex="0" role="button" href="https://raw.githubusercontent.com/NXPPlugNTrust/nano-package/master/examples/se05x_rotate_scp03_keys/src/ex_se05x_rotate_scp03_keys.c" rel="noreferrer" aria-expanded="false" aria-haspopup="dialog" data-base-ui-click-trigger="" data-label="2" aria-label="Citation 2" target="_blank"&gt;&lt;/A&gt;&lt;/P&gt;
&lt;DIV class="l8rrz21 _1ibi0s3en" data-ui-element="code-block-container"&gt;
&lt;PRE&gt;&lt;CODE class="markdown-code-c p8i6j0e hljs language-c _12n1b832"&gt;&lt;SPAN class="hljs-type"&gt;uint8_t&lt;/SPAN&gt; NEW_scp03_enc_key[AES_KEY_LEN_nBYTE] = {
    &lt;SPAN class="hljs-number"&gt;0xbf&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xc2&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xdb&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xe1&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x82&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x8e&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x03&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x5d&lt;/SPAN&gt;,
    &lt;SPAN class="hljs-number"&gt;0x3e&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x7f&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xa3&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x6b&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x90&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x2a&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x05&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xc6&lt;/SPAN&gt; };

&lt;SPAN class="hljs-type"&gt;uint8_t&lt;/SPAN&gt; NEW_scp03_mac_key[AES_KEY_LEN_nBYTE] = {
    &lt;SPAN class="hljs-number"&gt;0xbe&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xf8&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x5b&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xd7&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xba&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x04&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x97&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xd6&lt;/SPAN&gt;,
    &lt;SPAN class="hljs-number"&gt;0x28&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x78&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x1c&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xe4&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x7b&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x18&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x8c&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x96&lt;/SPAN&gt; };

&lt;SPAN class="hljs-type"&gt;uint8_t&lt;/SPAN&gt; NEW_scp03_dek_key[AES_KEY_LEN_nBYTE] = {
    &lt;SPAN class="hljs-number"&gt;0xd8&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x73&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xf3&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x16&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xbe&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x29&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x7f&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x2f&lt;/SPAN&gt;,
    &lt;SPAN class="hljs-number"&gt;0xc9&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xc0&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0xe4&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x5f&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x54&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x71&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x06&lt;/SPAN&gt;, &lt;SPAN class="hljs-number"&gt;0x99&lt;/SPAN&gt; };
&lt;/CODE&gt;&lt;/PRE&gt;
&lt;DIV class="l8rrz23 _1ibi0s3dp _1ibi0s332 _1ibi0s3eo _1ibi0s3bm _1ibi0s3ce"&gt;
&lt;DIV class="l8rrz25 _1ibi0s3eb"&gt;c&lt;/DIV&gt;
&lt;DIV class="lqznwq0"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;H3 class="_9k2iva0 p8i6j0c _1ibi0s314 heading3 _9k2iva1"&gt;Change 3 — Comment out the revert block&lt;/H3&gt;
&lt;P class="p8i6j01 paragraph"&gt;In &lt;CODE class="p8i6j0f"&gt;ex_se05x_rotate_scp03_keys()&lt;/CODE&gt;, comment out lines 85–90 so the code does a &lt;STRONG&gt;single rotation only&lt;/STRONG&gt; (current → default) and does not try to rotate back again: &lt;A id="base-ui-:r4qf:" class="wdbi343 wdbi341 _1ibi0s3ec _1ibi0s376" tabindex="0" role="button" href="https://raw.githubusercontent.com/NXPPlugNTrust/nano-package/master/examples/se05x_rotate_scp03_keys/src/ex_se05x_rotate_scp03_keys.c" rel="noreferrer" aria-expanded="false" aria-haspopup="dialog" data-base-ui-click-trigger="" data-label="2" aria-label="Citation 2" target="_blank"&gt;&lt;/A&gt;&lt;/P&gt;
&lt;DIV class="l8rrz21 _1ibi0s3en" data-ui-element="code-block-container"&gt;
&lt;PRE&gt;&lt;CODE class="markdown-code-c p8i6j0e hljs language-c _12n1b832"&gt;&lt;SPAN class="hljs-comment"&gt;/* -- Comment out the revert block below -- */&lt;/SPAN&gt;
&lt;SPAN class="hljs-comment"&gt;// SMLOG_I("Reverting SCP03 keys(version - %02x) to OLD KEYS \n", KEY_VERSION);&lt;/SPAN&gt;
&lt;SPAN class="hljs-comment"&gt;// ret = ex_se05x_change_keys(&amp;amp;se05x_session, &amp;amp;scp03_enc_key[0], &amp;amp;scp03_mac_key[0], &amp;amp;scp03_dek_key[0]);&lt;/SPAN&gt;
&lt;SPAN class="hljs-comment"&gt;// if (ret != 0) {&lt;/SPAN&gt;
&lt;SPAN class="hljs-comment"&gt;//     SMLOG_E("Error in ex_se05x_change_keys \n");&lt;/SPAN&gt;
&lt;SPAN class="hljs-comment"&gt;//     return 1;&lt;/SPAN&gt;
&lt;SPAN class="hljs-comment"&gt;// }&lt;/SPAN&gt;
&lt;/CODE&gt;&lt;/PRE&gt;
&lt;DIV class="l8rrz23 _1ibi0s3dp _1ibi0s332 _1ibi0s3eo _1ibi0s3bm _1ibi0s3ce"&gt;
&lt;DIV class="l8rrz25 _1ibi0s3eb"&gt;c&lt;/DIV&gt;
&lt;DIV class="lqznwq0"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;H2 class="_9k2iva0 p8i6j0c _1ibi0s314 heading2 _9k2iva1"&gt;&amp;nbsp;&lt;/H2&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 04 Sep 2026 08:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/How-to-revert-Platform-SCP03-keys-back-to-default-using-se05x-TP/m-p/2411228#M2150</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2026-09-04T08:24:38Z</dc:date>
    </item>
  </channel>
</rss>