<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure Authentication中的主题 ntag424的Originality Signature</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/ntag424%E7%9A%84Originality-Signature/m-p/2400290#M2119</link>
    <description>&lt;P&gt;你好：&lt;/P&gt;&lt;P&gt;我司已经签署保密协议，但是不知道如何使用natg424 uid与公钥，Read_Sig获取的56字节签名在嵌入式硬件平台实现ECDSA验证。文档上an11350没有详细步骤实现ECDSA verification(secp224r1),能否告诉我申请哪些资料来实现，谢谢。&lt;/P&gt;</description>
    <pubDate>Thu, 30 Jul 2026 02:05:19 GMT</pubDate>
    <dc:creator>qinzhi</dc:creator>
    <dc:date>2026-07-30T02:05:19Z</dc:date>
    <item>
      <title>ntag424的Originality Signature</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/ntag424%E7%9A%84Originality-Signature/m-p/2400290#M2119</link>
      <description>&lt;P&gt;你好：&lt;/P&gt;&lt;P&gt;我司已经签署保密协议，但是不知道如何使用natg424 uid与公钥，Read_Sig获取的56字节签名在嵌入式硬件平台实现ECDSA验证。文档上an11350没有详细步骤实现ECDSA verification(secp224r1),能否告诉我申请哪些资料来实现，谢谢。&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jul 2026 02:05:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/ntag424%E7%9A%84Originality-Signature/m-p/2400290#M2119</guid>
      <dc:creator>qinzhi</dc:creator>
      <dc:date>2026-07-30T02:05:19Z</dc:date>
    </item>
    <item>
      <title>Re: ntag424的Originality Signature</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/ntag424%E7%9A%84Originality-Signature/m-p/2400593#M2120</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/265153"&gt;@qinzhi&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;My apologies, the Application Note that is used as reference for NTAG Signature Validation (AN11350) is intended for other NTAG products holding 32-byte signature and different curves.&lt;/P&gt;
&lt;P&gt;Available procedure for asymmetric signature verification is described in &lt;A href="https://www.nxp.com/docs/en/application-note/AN12196.pdf" target="_blank"&gt;NTAG 424 DNA and NTAG 424 DNA TagTamper features and hints&lt;/A&gt;, Section 7.2. However, there is no information specific to ECDSA verification as this procedure is done outside the card.&lt;/P&gt;
&lt;P&gt;I apologize again for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jul 2026 17:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/ntag424%E7%9A%84Originality-Signature/m-p/2400593#M2120</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-07-30T17:24:59Z</dc:date>
    </item>
  </channel>
</rss>