<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: EdgeLock SE050/SE051 Capability Inquiry for Ed25519/X25519-Based IoT Device</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/EdgeLock-SE050-SE051-Capability-Inquiry-for-Ed25519-X25519-Based/m-p/2388795#M2106</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264045"&gt;@SahilPai&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please kindly have my comments as below:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;1. Key Storage&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can the SE050/SE051 securely store non-exportable private keys? //Yes, private keys are non-exportable on SE05x.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can certificates and public keys be stored in the secure element? // Yes, certs are stored as binary files within the SE , and public key can be stored standalone or together with the private key in SE05x.&lt;BR /&gt;&lt;BR /&gt;2. Key Generation&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can the secure element generate key pairs internally?// Yes, it supports.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Specifically, does it support generation of Ed25519 and X25519 key pairs within the secure element?// Yes,&amp;nbsp;Ed25519 and X25519 key pairs are supported.&lt;BR /&gt;&lt;BR /&gt;3. Ed25519 Operations&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can Ed25519 signing and signature verification be supported inside the secure element?// Yes, Ed25519 signing and signature verification are supported inside the SE05x.&lt;BR /&gt;&lt;BR /&gt;4. X25519 Operations&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can X25519 key agreement (ECDH shared secret computation) be performed inside the secure element using a non-exportable private key? //Yes, ECDH is performed with a private key within SE05x and an external&amp;nbsp; public key which can be stored in SE05x as well.&lt;BR /&gt;&lt;BR /&gt;5. AES Operations&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp; &amp;nbsp;- Does the secure element support AES encryption and decryption operations? //Yes,&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - If so, which AES modes are supported?//&amp;nbsp;Support for AES Modes:CBC, ECB, CTR, GCM, CCM.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;6. Storage read/write&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp; &amp;nbsp;- Storing/removing/accessing files like wifi passwords?//Yes,&amp;nbsp;&lt;SPAN&gt;SE050/SE051 can store binary objects in its secure object store, including&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Wi-Fi credentials.&lt;/SPAN&gt;&lt;/DIV&gt;
&lt;DIV&gt;&lt;BR /&gt;7. Linux / Raspberry Pi Integration&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Is there an SDK or middleware available for Raspberry Pi OS?// Yes, please refer to&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=SE05x-PLUG-TRUST-MW&amp;amp;appType=license" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=SE05x-PLUG-TRUST-MW&amp;amp;appType=license&lt;/A&gt;&amp;nbsp;for details.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Are there example applications demonstrating the above operations?//Yes.&lt;BR /&gt;&lt;BR /&gt;8. Product Selection&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Which EdgeLock SE050/SE051 variant would you recommend for the above requirements?// Either SE050E2 or SE051C2 can be used.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - What are the major differences between the recommended variants?// They both have the latest applet version, but SE051 supports applet upgrade while SE050 doesn't.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Are there any newer EdgeLock products that would be a better fit for these requirements?//not yet so far.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/products/SE050" target="_blank"&gt;https://www.nxp.com/products/SE050&lt;/A&gt;&amp;nbsp;and&amp;nbsp;&lt;A href="https://www.nxp.com/products/SE051" target="_blank"&gt;https://www.nxp.com/products/SE051&lt;/A&gt;&amp;nbsp;for more details.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Hope that helps,&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;/DIV&gt;</description>
    <pubDate>Wed, 01 Jul 2026 06:45:20 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2026-07-01T06:45:20Z</dc:date>
    <item>
      <title>EdgeLock SE050/SE051 Capability Inquiry for Ed25519/X25519-Based IoT Device</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/EdgeLock-SE050-SE051-Capability-Inquiry-for-Ed25519-X25519-Based/m-p/2385108#M2105</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello NXP Team,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We are evaluating the EdgeLock SE050/SE051 family for a Raspberry Pi based IoT device and would appreciate guidance on the most suitable part number.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Our primary requirements are secure storage and hardware execution of cryptographic operations.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;The device is a Raspberry Pi 4 - running Raspberry Pi OS (Linux).&lt;BR /&gt;&lt;BR /&gt;We would like clarification on the following points:&lt;BR /&gt;&lt;BR /&gt;1. Key Storage&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can the SE050/SE051 securely store non-exportable private keys?&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can certificates and public keys be stored in the secure element?&lt;BR /&gt;&lt;BR /&gt;2. Key Generation&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can the secure element generate key pairs internally?&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Specifically, does it support generation of Ed25519 and X25519 key pairs within the secure element?&lt;BR /&gt;&lt;BR /&gt;3. Ed25519 Operations&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can Ed25519 signing and signature verification be supported inside the secure element?&lt;BR /&gt;&lt;BR /&gt;4. X25519 Operations&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can X25519 key agreement (ECDH shared secret computation) be performed inside the secure element using a non-exportable private key?&lt;BR /&gt;&lt;BR /&gt;5. AES Operations&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; &amp;nbsp;- Does the secure element support AES encryption and decryption operations?&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - If so, which AES modes are supported?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;6. Storage read/write&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; &amp;nbsp;- Storing/removing/accessing files like wifi passwords?&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;7. Linux / Raspberry Pi Integration&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Is there an SDK or middleware available for Raspberry Pi OS?&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Are there example applications demonstrating the above operations?&lt;BR /&gt;&lt;BR /&gt;8. Product Selection&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Which EdgeLock SE050/SE051 variant would you recommend for the above requirements?&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - What are the major differences between the recommended variants?&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Are there any newer EdgeLock products that would be a better fit for these requirements?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;Our intended use case is:&lt;BR /&gt;&lt;BR /&gt;- Ed25519 signing for device authentication / JWT generation&lt;BR /&gt;- X25519 key agreement for mobile-device provisioning&lt;BR /&gt;- AES encryption/decryption using derived session keys&lt;/DIV&gt;&lt;DIV&gt;- Storage and handling of security files like Wifi passwords etc&lt;BR /&gt;- Large-scale deployment of IoT devices&lt;BR /&gt;&lt;BR /&gt;If available, we would also appreciate links to any of these:&lt;BR /&gt;&lt;BR /&gt;- Relevant datasheets&lt;BR /&gt;- Application notes&lt;BR /&gt;- SDK documentation&lt;BR /&gt;- Evaluation boards&lt;BR /&gt;- Linux/Raspberry Pi examples&lt;BR /&gt;&lt;BR /&gt;Thank you for your assistance.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Sahil Pai&lt;/DIV&gt;</description>
      <pubDate>Tue, 23 Jun 2026 13:53:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/EdgeLock-SE050-SE051-Capability-Inquiry-for-Ed25519-X25519-Based/m-p/2385108#M2105</guid>
      <dc:creator>SahilPai</dc:creator>
      <dc:date>2026-06-23T13:53:00Z</dc:date>
    </item>
    <item>
      <title>Re: EdgeLock SE050/SE051 Capability Inquiry for Ed25519/X25519-Based IoT Device</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/EdgeLock-SE050-SE051-Capability-Inquiry-for-Ed25519-X25519-Based/m-p/2388795#M2106</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264045"&gt;@SahilPai&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please kindly have my comments as below:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;1. Key Storage&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can the SE050/SE051 securely store non-exportable private keys? //Yes, private keys are non-exportable on SE05x.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can certificates and public keys be stored in the secure element? // Yes, certs are stored as binary files within the SE , and public key can be stored standalone or together with the private key in SE05x.&lt;BR /&gt;&lt;BR /&gt;2. Key Generation&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can the secure element generate key pairs internally?// Yes, it supports.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Specifically, does it support generation of Ed25519 and X25519 key pairs within the secure element?// Yes,&amp;nbsp;Ed25519 and X25519 key pairs are supported.&lt;BR /&gt;&lt;BR /&gt;3. Ed25519 Operations&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can Ed25519 signing and signature verification be supported inside the secure element?// Yes, Ed25519 signing and signature verification are supported inside the SE05x.&lt;BR /&gt;&lt;BR /&gt;4. X25519 Operations&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Can X25519 key agreement (ECDH shared secret computation) be performed inside the secure element using a non-exportable private key? //Yes, ECDH is performed with a private key within SE05x and an external&amp;nbsp; public key which can be stored in SE05x as well.&lt;BR /&gt;&lt;BR /&gt;5. AES Operations&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp; &amp;nbsp;- Does the secure element support AES encryption and decryption operations? //Yes,&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - If so, which AES modes are supported?//&amp;nbsp;Support for AES Modes:CBC, ECB, CTR, GCM, CCM.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;6. Storage read/write&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp; &amp;nbsp;- Storing/removing/accessing files like wifi passwords?//Yes,&amp;nbsp;&lt;SPAN&gt;SE050/SE051 can store binary objects in its secure object store, including&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Wi-Fi credentials.&lt;/SPAN&gt;&lt;/DIV&gt;
&lt;DIV&gt;&lt;BR /&gt;7. Linux / Raspberry Pi Integration&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Is there an SDK or middleware available for Raspberry Pi OS?// Yes, please refer to&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=SE05x-PLUG-TRUST-MW&amp;amp;appType=license" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=SE05x-PLUG-TRUST-MW&amp;amp;appType=license&lt;/A&gt;&amp;nbsp;for details.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Are there example applications demonstrating the above operations?//Yes.&lt;BR /&gt;&lt;BR /&gt;8. Product Selection&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Which EdgeLock SE050/SE051 variant would you recommend for the above requirements?// Either SE050E2 or SE051C2 can be used.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - What are the major differences between the recommended variants?// They both have the latest applet version, but SE051 supports applet upgrade while SE050 doesn't.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Are there any newer EdgeLock products that would be a better fit for these requirements?//not yet so far.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/products/SE050" target="_blank"&gt;https://www.nxp.com/products/SE050&lt;/A&gt;&amp;nbsp;and&amp;nbsp;&lt;A href="https://www.nxp.com/products/SE051" target="_blank"&gt;https://www.nxp.com/products/SE051&lt;/A&gt;&amp;nbsp;for more details.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Hope that helps,&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Wed, 01 Jul 2026 06:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/EdgeLock-SE050-SE051-Capability-Inquiry-for-Ed25519-X25519-Based/m-p/2388795#M2106</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2026-07-01T06:45:20Z</dc:date>
    </item>
  </channel>
</rss>