<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Generate Private RSA key Inside SE052 in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Generate-Private-RSA-key-Inside-SE052/m-p/2382586#M2093</link>
    <description>&lt;P&gt;I use SE052 Secuere element IC.&lt;BR /&gt;I create zephyr based sample application which is generates RSA private key inside SE052.&lt;BR /&gt;But face the issue to generate new private RSA key, check this logs and fix it.&lt;BR /&gt;I want to Generate RSA key inside SE052 which can be use for TLS handshake process.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;board is ESP32c3devkitm.&lt;BR /&gt;Zephyr RTOS version is 3.7.0 and TLS handshake v.1.2 is use.&lt;BR /&gt;I attach also sample application and logs with you. Please suggest how to generate RSA key.&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Logs are in .c file key_generation_failed.c file&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jun 2026 15:14:06 GMT</pubDate>
    <dc:creator>MohitGediya</dc:creator>
    <dc:date>2026-06-17T15:14:06Z</dc:date>
    <item>
      <title>Generate Private RSA key Inside SE052</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Generate-Private-RSA-key-Inside-SE052/m-p/2382586#M2093</link>
      <description>&lt;P&gt;I use SE052 Secuere element IC.&lt;BR /&gt;I create zephyr based sample application which is generates RSA private key inside SE052.&lt;BR /&gt;But face the issue to generate new private RSA key, check this logs and fix it.&lt;BR /&gt;I want to Generate RSA key inside SE052 which can be use for TLS handshake process.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;board is ESP32c3devkitm.&lt;BR /&gt;Zephyr RTOS version is 3.7.0 and TLS handshake v.1.2 is use.&lt;BR /&gt;I attach also sample application and logs with you. Please suggest how to generate RSA key.&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Logs are in .c file key_generation_failed.c file&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jun 2026 15:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Generate-Private-RSA-key-Inside-SE052/m-p/2382586#M2093</guid>
      <dc:creator>MohitGediya</dc:creator>
      <dc:date>2026-06-17T15:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Private RSA key Inside SE052</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Generate-Private-RSA-key-Inside-SE052/m-p/2382587#M2094</link>
      <description>&lt;P&gt;Function defination of called function is in last and it's comment for your reference.&lt;BR /&gt;Is there any issue about associated keyID?&lt;BR /&gt;Or APDU command header.&lt;BR /&gt;Can i generate only private key or key_pair in any format. There is no issue about type.&lt;BR /&gt;I just want any type of private RSA key inside SE052.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jun 2026 15:17:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Generate-Private-RSA-key-Inside-SE052/m-p/2382587#M2094</guid>
      <dc:creator>MohitGediya</dc:creator>
      <dc:date>2026-06-17T15:17:49Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Private RSA key Inside SE052</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Generate-Private-RSA-key-Inside-SE052/m-p/2382848#M2095</link>
      <description>&lt;P&gt;Please reply&amp;nbsp;&lt;LI-MESSAGE title="MbedTLS Server connection with client using SE052" uid="2370197" url="https://community.nxp.com/t5/Secure-Authentication/MbedTLS-Server-connection-with-client-using-SE052/m-p/2370197#U2370197" discussion_style_icon_css="lia-mention-container-editor-message lia-img-icon-forum-thread lia-fa-icon lia-fa-forum lia-fa-thread lia-fa"&gt;&lt;/LI-MESSAGE&gt;&amp;nbsp;&lt;LI-MESSAGE title="MbedTLS v.1.2 handshake" uid="2374365" url="https://community.nxp.com/t5/Secure-Authentication/MbedTLS-v-1-2-handshake/m-p/2374365#U2374365" discussion_style_icon_css="lia-mention-container-editor-message lia-img-icon-forum-thread lia-fa-icon lia-fa-forum lia-fa-thread lia-fa"&gt;&lt;/LI-MESSAGE&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jun 2026 04:27:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Generate-Private-RSA-key-Inside-SE052/m-p/2382848#M2095</guid>
      <dc:creator>MohitGediya</dc:creator>
      <dc:date>2026-06-18T04:27:30Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Private RSA key Inside SE052</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Generate-Private-RSA-key-Inside-SE052/m-p/2382854#M2096</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262552"&gt;@MohitGediya&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please use&amp;nbsp;Se05x_API_WriteRSAKey() to generate the RSA key, the sample code can be something like below:&lt;/P&gt;
&lt;P&gt;status = Se05x_API_WriteRSAKey(pSe05xSession,&lt;BR /&gt;(Se05xPolicy_t *)&amp;amp;policy_for_auth_obj,&lt;BR /&gt;RSA_ATTESTATION_KEY_ID,&lt;BR /&gt;2048,&lt;BR /&gt;SE05X_RSA_NO_p,&lt;BR /&gt;SE05X_RSA_NO_q,&lt;BR /&gt;SE05X_RSA_NO_dp,&lt;BR /&gt;SE05X_RSA_NO_dq,&lt;BR /&gt;SE05X_RSA_NO_qInv,&lt;BR /&gt;SE05X_RSA_NO_pubExp,&lt;BR /&gt;SE05X_RSA_NO_priv,&lt;BR /&gt;SE05X_RSA_NO_pubMod,&lt;BR /&gt;kSE05x_INS_NA,&lt;BR /&gt;kSE05x_KeyPart_Pair,&lt;BR /&gt;kSE05x_RSAKeyFormat_CRT);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please assign proper policy to the key pair, especially no disabling the deletion, otherwise the key can not be removed any more.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jun 2026 04:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Generate-Private-RSA-key-Inside-SE052/m-p/2382854#M2096</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2026-06-18T04:50:43Z</dc:date>
    </item>
  </channel>
</rss>