<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックOpenSSL Provider with SE052F for RNG</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/OpenSSL-Provider-with-SE052F-for-RNG/m-p/2365478#M2074</link>
    <description>&lt;P&gt;We have a requirement to use the SE052F as a FIPS compliant source for random number generation. We require OpenSSL to use the SE052F, and in turn, all applications that use the openssl libraries to use the SE052F for RNG.&lt;/P&gt;&lt;P&gt;I understand we must use the NXP MW accessManager and the OpenSSL Provider.&lt;BR /&gt;I am using: SE-PLUG-TRUST-MW_04.07.01&lt;BR /&gt;I have followed the instructions in:&lt;BR /&gt;AN14028.pdf&lt;BR /&gt;SE-PLUG-TRUST-MW_04.07.01/simw-top/doc/hostlib/hostLib/accessManager/doc/accessManager.html&lt;BR /&gt;and the README info here (but not using this repo): &lt;A href="https://github.com/NXPPlugNTrust/se05x-openssl-provider" target="_blank"&gt;https://github.com/NXPPlugNTrust/se05x-openssl-provider&lt;/A&gt;&lt;/P&gt;&lt;P&gt;accessManager built with the following cmake options:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;NXP_SE_MW_CONF_OPTS += -DWithSharedLIB=OFF -DPTMW_Host=Raspbian -DPTMW_SMCOM=T1oI2C -DPTMW_Applet=SE05X_C \
	-DPTMW_FIPS=None -DPTMW_SE05X_Ver=07_02 -DPTMW_SE05X_Auth=PlatfSCP03 -DPTMW_SCP=SCP03_SSS -DSE05X_EN_PIN=582 -DSE_RESET_LOGIC=0 \
	-DPAHO_BUILD_SHARED=FALSE -DPAHO_BUILD_STATIC=TRUE&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;OpenSSL Provider built with the following cmake options:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;NXP_SE_MW2_CONF_OPTS += -DWithSharedLIB=ON -DPTMW_HostCrypto=OPENSSL -DPTMW_Host=Raspbian -DPTMW_SMCOM=JRCP_V1_AM -DPTMW_SE05X_Auth=None&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;openssl.cnf modified as follows:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[provider_sect]
nxp_prov = nxp_sect
default = default_sect

[nxp_sect]
identity = nxp_prov
module = /usr/lib/libsssProvider.so
activate = 1

[default_sect]
activate = 1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The accessManager starts:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Starting accessManager (Rev.1.1).
  Protect Link between accessManager and SE: YES.
accessManager JRCPv1 (T1oI2C SE side)
******************************************************************************
Server: waiting for connections on port 8040.
Server: only localhost based processes can connect.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;RNG using openssl from the command line seems to work OK:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# openssl rand -hex 64
sssprov-dbg: Enter - OSSL_provider_init 
App   :INFO :Using PortName='127.0.0.1:8040' (gszSocketPortDefault)
App   :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
New client connection from 127.0.0.1. Client ID: 5
Command 0x00 from client 5
DUMMY_ATR=0x01.A0.00.00.03.96.04.03.E8.00.FE.02.0B.03.E8.00.01.00.00.00.00.64.13.88.0A.00.65.53.45.30.35.31.00.00.00.
Replacing *_ATR by default (pre-cooked) ATR.
ATR=0x3B.FB.18.00.00.81.31.FE.45.50.4C.41.43.45.48.4F.4C.44.45.52.AB.
Command 0x01 from client 5
SM_EstablishPlatformSCP03Am (Entry)
App   :WARN :Using SCP03 keys from:'/tmp/SE05X/plain_scp.txt' (FILE=/tmp/SE05X/plain_scp.txt)
SE051 connected.
SM_EstablishPlatformSCP03Am (Exit); Status = 0x9000
sss   :INFO :Newer version of Applet Found
sss   :INFO :Compiled for 0x70200. Got newer 0x70216
sss   :WARN :Communication channel is Plain.
sss   :WARN :!!!Not recommended for production use.!!!
sssprov-dbg: Enter - sss_rand_newctx 
sssprov-dbg: Enter - sss_rand_instantiate 
sssprov-dbg: Enter - sss_rand_enable_locking 
sssprov-dbg: Enter - sss_rand_newctx 
sssprov-dbg: Enter - sss_rand_instantiate 
sssprov-dbg: Enter - sss_rand_get_ctx_params 
sssprov-dbg: Enter - sss_rand_generate 
sssprov-flw: Get random data from SE05x 
Command 0x01 from client 5
SM_SendAPDUAm: smStatus = 0x9000
5f0f4d63e4ec771b8cfd46dd50c497b7e4e56e203ad5bc6eca9f8c28d23f39aa2d4a807915e3c60cf2e6a833794cb1208554f3e635811354eadd7b2c911c60da
sssprov-dbg: Enter - sss_rand_freectx 
sssprov-dbg: Enter - sss_rand_freectx 
sssprov-dbg: Enter - sss_teardown 
Received 0 byte from client 5 (Message Header Phase) .&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But, starting the ssh daemon fails:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# /usr/sbin/sshd &amp;amp;
sssprov-dbg: Enter - OSSL_provider_init 
App   :INFO :Using PortName='127.0.0.1:8040' (gszSocketPortDefault)
App   :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
New client connection from 127.0.0.1. Client ID: 5
Command 0x00 from client 5
ATR=0x3B.FB.18.00.00.81.31.FE.45.50.4C.41.43.45.48.4F.4C.44.45.52.AB.
Command 0x01 from client 5
Pre-cooked response (rspAppletSelect)
sss   :INFO :Newer version of Applet Found
sss   :INFO :Compiled for 0x70200. Got newer 0x70216
sss   :WARN :Communication channel is Plain.
sss   :WARN :!!!Not recommended for production use.!!!
sssprov-dbg: Enter - sss_rand_newctx 
sssprov-dbg: Enter - sss_rand_instantiate 
sssprov-dbg: Enter - sss_rand_enable_locking 
sssprov-dbg: Enter - sss_rand_get_ctx_params 
PRNG is not seeded
Received 0 byte from client 5 (Message Header Phase) .
[2]+  Done(255)                  /usr/sbin/sshd&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd be very grateful for any help,&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 14 May 2026 10:42:53 GMT</pubDate>
    <dc:creator>sam123</dc:creator>
    <dc:date>2026-05-14T10:42:53Z</dc:date>
    <item>
      <title>OpenSSL Provider with SE052F for RNG</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/OpenSSL-Provider-with-SE052F-for-RNG/m-p/2365478#M2074</link>
      <description>&lt;P&gt;We have a requirement to use the SE052F as a FIPS compliant source for random number generation. We require OpenSSL to use the SE052F, and in turn, all applications that use the openssl libraries to use the SE052F for RNG.&lt;/P&gt;&lt;P&gt;I understand we must use the NXP MW accessManager and the OpenSSL Provider.&lt;BR /&gt;I am using: SE-PLUG-TRUST-MW_04.07.01&lt;BR /&gt;I have followed the instructions in:&lt;BR /&gt;AN14028.pdf&lt;BR /&gt;SE-PLUG-TRUST-MW_04.07.01/simw-top/doc/hostlib/hostLib/accessManager/doc/accessManager.html&lt;BR /&gt;and the README info here (but not using this repo): &lt;A href="https://github.com/NXPPlugNTrust/se05x-openssl-provider" target="_blank"&gt;https://github.com/NXPPlugNTrust/se05x-openssl-provider&lt;/A&gt;&lt;/P&gt;&lt;P&gt;accessManager built with the following cmake options:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;NXP_SE_MW_CONF_OPTS += -DWithSharedLIB=OFF -DPTMW_Host=Raspbian -DPTMW_SMCOM=T1oI2C -DPTMW_Applet=SE05X_C \
	-DPTMW_FIPS=None -DPTMW_SE05X_Ver=07_02 -DPTMW_SE05X_Auth=PlatfSCP03 -DPTMW_SCP=SCP03_SSS -DSE05X_EN_PIN=582 -DSE_RESET_LOGIC=0 \
	-DPAHO_BUILD_SHARED=FALSE -DPAHO_BUILD_STATIC=TRUE&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;OpenSSL Provider built with the following cmake options:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;NXP_SE_MW2_CONF_OPTS += -DWithSharedLIB=ON -DPTMW_HostCrypto=OPENSSL -DPTMW_Host=Raspbian -DPTMW_SMCOM=JRCP_V1_AM -DPTMW_SE05X_Auth=None&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;openssl.cnf modified as follows:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[provider_sect]
nxp_prov = nxp_sect
default = default_sect

[nxp_sect]
identity = nxp_prov
module = /usr/lib/libsssProvider.so
activate = 1

[default_sect]
activate = 1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The accessManager starts:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Starting accessManager (Rev.1.1).
  Protect Link between accessManager and SE: YES.
accessManager JRCPv1 (T1oI2C SE side)
******************************************************************************
Server: waiting for connections on port 8040.
Server: only localhost based processes can connect.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;RNG using openssl from the command line seems to work OK:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# openssl rand -hex 64
sssprov-dbg: Enter - OSSL_provider_init 
App   :INFO :Using PortName='127.0.0.1:8040' (gszSocketPortDefault)
App   :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
New client connection from 127.0.0.1. Client ID: 5
Command 0x00 from client 5
DUMMY_ATR=0x01.A0.00.00.03.96.04.03.E8.00.FE.02.0B.03.E8.00.01.00.00.00.00.64.13.88.0A.00.65.53.45.30.35.31.00.00.00.
Replacing *_ATR by default (pre-cooked) ATR.
ATR=0x3B.FB.18.00.00.81.31.FE.45.50.4C.41.43.45.48.4F.4C.44.45.52.AB.
Command 0x01 from client 5
SM_EstablishPlatformSCP03Am (Entry)
App   :WARN :Using SCP03 keys from:'/tmp/SE05X/plain_scp.txt' (FILE=/tmp/SE05X/plain_scp.txt)
SE051 connected.
SM_EstablishPlatformSCP03Am (Exit); Status = 0x9000
sss   :INFO :Newer version of Applet Found
sss   :INFO :Compiled for 0x70200. Got newer 0x70216
sss   :WARN :Communication channel is Plain.
sss   :WARN :!!!Not recommended for production use.!!!
sssprov-dbg: Enter - sss_rand_newctx 
sssprov-dbg: Enter - sss_rand_instantiate 
sssprov-dbg: Enter - sss_rand_enable_locking 
sssprov-dbg: Enter - sss_rand_newctx 
sssprov-dbg: Enter - sss_rand_instantiate 
sssprov-dbg: Enter - sss_rand_get_ctx_params 
sssprov-dbg: Enter - sss_rand_generate 
sssprov-flw: Get random data from SE05x 
Command 0x01 from client 5
SM_SendAPDUAm: smStatus = 0x9000
5f0f4d63e4ec771b8cfd46dd50c497b7e4e56e203ad5bc6eca9f8c28d23f39aa2d4a807915e3c60cf2e6a833794cb1208554f3e635811354eadd7b2c911c60da
sssprov-dbg: Enter - sss_rand_freectx 
sssprov-dbg: Enter - sss_rand_freectx 
sssprov-dbg: Enter - sss_teardown 
Received 0 byte from client 5 (Message Header Phase) .&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But, starting the ssh daemon fails:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# /usr/sbin/sshd &amp;amp;
sssprov-dbg: Enter - OSSL_provider_init 
App   :INFO :Using PortName='127.0.0.1:8040' (gszSocketPortDefault)
App   :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
New client connection from 127.0.0.1. Client ID: 5
Command 0x00 from client 5
ATR=0x3B.FB.18.00.00.81.31.FE.45.50.4C.41.43.45.48.4F.4C.44.45.52.AB.
Command 0x01 from client 5
Pre-cooked response (rspAppletSelect)
sss   :INFO :Newer version of Applet Found
sss   :INFO :Compiled for 0x70200. Got newer 0x70216
sss   :WARN :Communication channel is Plain.
sss   :WARN :!!!Not recommended for production use.!!!
sssprov-dbg: Enter - sss_rand_newctx 
sssprov-dbg: Enter - sss_rand_instantiate 
sssprov-dbg: Enter - sss_rand_enable_locking 
sssprov-dbg: Enter - sss_rand_get_ctx_params 
PRNG is not seeded
Received 0 byte from client 5 (Message Header Phase) .
[2]+  Done(255)                  /usr/sbin/sshd&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd be very grateful for any help,&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 May 2026 10:42:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/OpenSSL-Provider-with-SE052F-for-RNG/m-p/2365478#M2074</guid>
      <dc:creator>sam123</dc:creator>
      <dc:date>2026-05-14T10:42:53Z</dc:date>
    </item>
    <item>
      <title>Re: OpenSSL Provider with SE052F for RNG</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/OpenSSL-Provider-with-SE052F-for-RNG/m-p/2371152#M2077</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262765"&gt;@sam123&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The&amp;nbsp;Openssh support is not tested with our provider currently.&amp;nbsp;This needs to be analyzed further and may require changes. &amp;nbsp; An internal ticket was created for RnD and they will do analysis.&amp;nbsp; &amp;nbsp;I will let you know when I have any more info from there.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your patience!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 26 May 2026 08:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/OpenSSL-Provider-with-SE052F-for-RNG/m-p/2371152#M2077</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2026-05-26T08:15:34Z</dc:date>
    </item>
  </channel>
</rss>