<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to batch modify SCP03 KEY of SE05E? in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/How-to-batch-modify-SCP03-KEY-of-SE05E/m-p/2248789#M1945</link>
    <description>&lt;P&gt;Dear Kan,&lt;/P&gt;&lt;P&gt;&amp;nbsp; The customer wants to know how to batch modify the SCP03 KEY of SE050E. Have they encountered such cases in previous users? Do you have any good suggestions?&lt;/P&gt;&lt;P&gt;For example, do users need to design the board themselves and modify it using the touch points and software methods on it? Is this feasible？&lt;/P&gt;&lt;P&gt;Looking forward to your reply！&lt;/P&gt;&lt;P&gt;Best Wishes！&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 26 Nov 2025 02:18:38 GMT</pubDate>
    <dc:creator>Nancy_LAN</dc:creator>
    <dc:date>2025-11-26T02:18:38Z</dc:date>
    <item>
      <title>How to batch modify SCP03 KEY of SE05E?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/How-to-batch-modify-SCP03-KEY-of-SE05E/m-p/2248789#M1945</link>
      <description>&lt;P&gt;Dear Kan,&lt;/P&gt;&lt;P&gt;&amp;nbsp; The customer wants to know how to batch modify the SCP03 KEY of SE050E. Have they encountered such cases in previous users? Do you have any good suggestions?&lt;/P&gt;&lt;P&gt;For example, do users need to design the board themselves and modify it using the touch points and software methods on it? Is this feasible？&lt;/P&gt;&lt;P&gt;Looking forward to your reply！&lt;/P&gt;&lt;P&gt;Best Wishes！&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Nov 2025 02:18:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/How-to-batch-modify-SCP03-KEY-of-SE05E/m-p/2248789#M1945</guid>
      <dc:creator>Nancy_LAN</dc:creator>
      <dc:date>2025-11-26T02:18:38Z</dc:date>
    </item>
    <item>
      <title>Re: How to batch modify SCP03 KEY of SE05E?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/How-to-batch-modify-SCP03-KEY-of-SE05E/m-p/2248873#M1946</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241117"&gt;@Nancy_LAN&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To modify the SCP03 keys on SE050E , we recommend implementing it in the application code which holds the default SCP03 keys as well as the new keys, so the device may rotate the default keys with the new ones on the first power up. We provide rotating demo in the MW, and they may use it as a reference.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 26 Nov 2025 04:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/How-to-batch-modify-SCP03-KEY-of-SE05E/m-p/2248873#M1946</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2025-11-26T04:07:58Z</dc:date>
    </item>
  </channel>
</rss>