<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure Authenticationのトピックwriting PCR using ssscli</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/writing-PCR-using-ssscli/m-p/2038616#M1790</link>
    <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I just set up a test using an RPI3 and the SE050ARD-E evaluation board. I did some first tests using the ssscli tool and till now I managed to get some examples working, but what I can't figure out is how to create a PCR object and write and read to or from it.&lt;/P&gt;&lt;P&gt;I can run the "se05x_PCR" example, but I don't know how to do it using the ssscli tool?! Is this possible at all?&lt;/P&gt;</description>
    <pubDate>Wed, 05 Feb 2025 12:54:10 GMT</pubDate>
    <dc:creator>Henrik78</dc:creator>
    <dc:date>2025-02-05T12:54:10Z</dc:date>
    <item>
      <title>writing PCR using ssscli</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/writing-PCR-using-ssscli/m-p/2038616#M1790</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I just set up a test using an RPI3 and the SE050ARD-E evaluation board. I did some first tests using the ssscli tool and till now I managed to get some examples working, but what I can't figure out is how to create a PCR object and write and read to or from it.&lt;/P&gt;&lt;P&gt;I can run the "se05x_PCR" example, but I don't know how to do it using the ssscli tool?! Is this possible at all?&lt;/P&gt;</description>
      <pubDate>Wed, 05 Feb 2025 12:54:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/writing-PCR-using-ssscli/m-p/2038616#M1790</guid>
      <dc:creator>Henrik78</dc:creator>
      <dc:date>2025-02-05T12:54:10Z</dc:date>
    </item>
    <item>
      <title>Re: writing PCR using ssscli</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/writing-PCR-using-ssscli/m-p/2039752#M1793</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/246432"&gt;@Henrik78&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The ssscli doesn't support PCR, and this tool is recommended for develop purpose, but for production, you have to write application code based on the MW something like&amp;nbsp;&lt;SPAN&gt;se05x_PCR.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 07:05:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/writing-PCR-using-ssscli/m-p/2039752#M1793</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2025-02-07T07:05:49Z</dc:date>
    </item>
  </channel>
</rss>