<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic OM-SE050ARD-E and arduino - Kiloblitz? in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/OM-SE050ARD-E-and-arduino-Kiloblitz/m-p/2006469#M1766</link>
    <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I am working with the OM-SE050ARD-E development board and need guidance on configuring it to generate a secp256k1 elliptic curve key pair, specifically for Bitcoin Native SegWit address generation. While I understand that I need to use the Se05x_API_CreateCurve() function to initialize the curve, I want to make sure I get this right, as it’s a critical component of my project.&lt;/P&gt;&lt;P&gt;I am comfortable handling the Bitcoin-specific operations (e.g., public key compression, hashing, Bech32 encoding) using libraries like uBitcoin in Arduino. However, if I cannot properly configure the SE050 for secp256k1, I am essentially stuck.&lt;/P&gt;&lt;P&gt;Here are my specific questions:&lt;/P&gt;&lt;P&gt;What are the exact steps to configure the OM-SE050ARD-E for the secp256k1 curve using the NXP middleware?&lt;BR /&gt;Are there specific parameters or policies I should set during key generation to ensure secure, repeatable results?&lt;BR /&gt;Can the configuration process be repeated safely on the development board, or are there irreversible steps I should be cautious about?&lt;BR /&gt;Any example code or best practices would be invaluable. I want to ensure I fully utilize the SE050’s capabilities while minimizing risks during development.&lt;/P&gt;&lt;P&gt;Thank you for your help!&lt;/P&gt;</description>
    <pubDate>Wed, 04 Dec 2024 01:28:26 GMT</pubDate>
    <dc:creator>sick_cat</dc:creator>
    <dc:date>2024-12-04T01:28:26Z</dc:date>
    <item>
      <title>OM-SE050ARD-E and arduino - Kiloblitz?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/OM-SE050ARD-E-and-arduino-Kiloblitz/m-p/2006469#M1766</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I am working with the OM-SE050ARD-E development board and need guidance on configuring it to generate a secp256k1 elliptic curve key pair, specifically for Bitcoin Native SegWit address generation. While I understand that I need to use the Se05x_API_CreateCurve() function to initialize the curve, I want to make sure I get this right, as it’s a critical component of my project.&lt;/P&gt;&lt;P&gt;I am comfortable handling the Bitcoin-specific operations (e.g., public key compression, hashing, Bech32 encoding) using libraries like uBitcoin in Arduino. However, if I cannot properly configure the SE050 for secp256k1, I am essentially stuck.&lt;/P&gt;&lt;P&gt;Here are my specific questions:&lt;/P&gt;&lt;P&gt;What are the exact steps to configure the OM-SE050ARD-E for the secp256k1 curve using the NXP middleware?&lt;BR /&gt;Are there specific parameters or policies I should set during key generation to ensure secure, repeatable results?&lt;BR /&gt;Can the configuration process be repeated safely on the development board, or are there irreversible steps I should be cautious about?&lt;BR /&gt;Any example code or best practices would be invaluable. I want to ensure I fully utilize the SE050’s capabilities while minimizing risks during development.&lt;/P&gt;&lt;P&gt;Thank you for your help!&lt;/P&gt;</description>
      <pubDate>Wed, 04 Dec 2024 01:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/OM-SE050ARD-E-and-arduino-Kiloblitz/m-p/2006469#M1766</guid>
      <dc:creator>sick_cat</dc:creator>
      <dc:date>2024-12-04T01:28:26Z</dc:date>
    </item>
    <item>
      <title>Re: OM-SE050ARD-E and arduino - Kiloblitz?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/OM-SE050ARD-E-and-arduino-Kiloblitz/m-p/2006550#M1767</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244166"&gt;@sick_cat&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There have already been several threads on this topic, and for you case, you may refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/How-to-properly-parametrize-a-SECP256K1-curve-using-the-SE051/m-p/1810404#M21177" target="_blank"&gt;https://community.nxp.com/t5/Other-NXP-Products/How-to-properly-parametrize-a-SECP256K1-curve-using-the-SE051/m-p/1810404#M21177&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 04 Dec 2024 03:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/OM-SE050ARD-E-and-arduino-Kiloblitz/m-p/2006550#M1767</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-12-04T03:38:52Z</dc:date>
    </item>
  </channel>
</rss>