<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: Error messages with se5x when reading id list</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Error-messages-with-se5x-when-reading-id-list/m-p/2005443#M1764</link>
    <description>&lt;P&gt;Thanks for the suggestion.&lt;/P&gt;&lt;P&gt;I ended up getting it working by reprogramming my BSP. I didn't try the verbose log as I didn't have the time to do the setup for that. I suspect the problem was caused by corrupted files and not by anything to do with the chip or the i2c communication.&lt;/P&gt;</description>
    <pubDate>Mon, 02 Dec 2024 21:21:56 GMT</pubDate>
    <dc:creator>Jamier</dc:creator>
    <dc:date>2024-12-02T21:21:56Z</dc:date>
    <item>
      <title>Error messages with se5x when reading id list</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Error-messages-with-se5x-when-reading-id-list/m-p/1972339#M1722</link>
      <description>&lt;P&gt;I am working with a provisioned secure element se050 and I am suddenly getting error messages instead of the id list.&lt;/P&gt;&lt;P&gt;I use these commands and I would normally get an output of a bunch of key ids.&lt;/P&gt;&lt;P&gt;ssscli connect se05x t1oi2c non&lt;/P&gt;&lt;P&gt;ssscli se05x readidlist&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But suddenly I am seeing these two error messages on two different chips:&lt;/P&gt;&lt;P&gt;ERROR:cli.cli:invalid load key, '\x00'.&lt;BR /&gt;ERROR:cli.cli:'Context' object has no attribute 'session'&lt;/P&gt;&lt;P&gt;ERROR:cli.cli:Ran out of input&lt;BR /&gt;ERROR:cli.cli:'Context' object has no attribute 'session'&lt;/P&gt;&lt;P&gt;A power cycle doesn't help.&lt;/P&gt;&lt;P&gt;Does anyone know what's going on?&amp;nbsp;&lt;/P&gt;&lt;P&gt;The devices these chips have been installed on have been undergoing stress and environmental testing -40C to +65C.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Oct 2024 19:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Error-messages-with-se5x-when-reading-id-list/m-p/1972339#M1722</guid>
      <dc:creator>Jamier</dc:creator>
      <dc:date>2024-10-11T19:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: Error messages with se5x when reading id list</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Error-messages-with-se5x-when-reading-id-list/m-p/1973016#M1723</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/2172"&gt;@Jamier&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which variant of SE05x was used in your test? Have you tried to rebuild&amp;nbsp;&lt;SPAN&gt;sssapisw within the MW with the verbose log level? It would be very helpful to have the log during this issue.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1728886754904.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304474iC531EB3342CE2CA9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Kan_Li_0-1728886754904.png" alt="Kan_Li_0-1728886754904.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Kan_Li_0-1728886754904.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 06:19:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Error-messages-with-se5x-when-reading-id-list/m-p/1973016#M1723</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-10-14T06:19:51Z</dc:date>
    </item>
    <item>
      <title>Re: Error messages with se5x when reading id list</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Error-messages-with-se5x-when-reading-id-list/m-p/2005443#M1764</link>
      <description>&lt;P&gt;Thanks for the suggestion.&lt;/P&gt;&lt;P&gt;I ended up getting it working by reprogramming my BSP. I didn't try the verbose log as I didn't have the time to do the setup for that. I suspect the problem was caused by corrupted files and not by anything to do with the chip or the i2c communication.&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 21:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Error-messages-with-se5x-when-reading-id-list/m-p/2005443#M1764</guid>
      <dc:creator>Jamier</dc:creator>
      <dc:date>2024-12-02T21:21:56Z</dc:date>
    </item>
  </channel>
</rss>