<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure Authentication中的主题 Getting error 0x6985 with SE05x</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Getting-error-0x6985-with-SE05x/m-p/1961205#M1701</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the evaluation board for SE052. I'm trying to implement the se052_reset_example but it is not working. The function ex_sss_boot_open works fine and the applet is selected. However, the next command from &lt;SPAN&gt;Se05x_API_GetRandom function returns the error 0x6985.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I've also tried sending different commands after&amp;nbsp;ex_sss_boot_open, like&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Se05x_API_GetFreeMemory&amp;nbsp;but I received the same 0x6985 error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 25 Sep 2024 02:16:46 GMT</pubDate>
    <dc:creator>ar01</dc:creator>
    <dc:date>2024-09-25T02:16:46Z</dc:date>
    <item>
      <title>Getting error 0x6985 with SE05x</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Getting-error-0x6985-with-SE05x/m-p/1961205#M1701</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the evaluation board for SE052. I'm trying to implement the se052_reset_example but it is not working. The function ex_sss_boot_open works fine and the applet is selected. However, the next command from &lt;SPAN&gt;Se05x_API_GetRandom function returns the error 0x6985.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I've also tried sending different commands after&amp;nbsp;ex_sss_boot_open, like&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Se05x_API_GetFreeMemory&amp;nbsp;but I received the same 0x6985 error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Sep 2024 02:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Getting-error-0x6985-with-SE05x/m-p/1961205#M1701</guid>
      <dc:creator>ar01</dc:creator>
      <dc:date>2024-09-25T02:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: Getting error 0x6985 with SE05x</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Getting-error-0x6985-with-SE05x/m-p/1961486#M1702</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239453"&gt;@ar01&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Actually&amp;nbsp;the SE052F uses like SE050F a mandated PlatformSCP connection. Did you configure the MW correctly ? Please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN14028" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=AN14028&lt;/A&gt;&amp;nbsp;for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 25 Sep 2024 07:48:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Getting-error-0x6985-with-SE05x/m-p/1961486#M1702</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-09-25T07:48:17Z</dc:date>
    </item>
    <item>
      <title>Re: Getting error 0x6985 with SE05x</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Getting-error-0x6985-with-SE05x/m-p/1962055#M1703</link>
      <description>Thanks Kan!, I thought that was disabled by default, I changed the features to include the platform scp and that worked. Have a nice day.</description>
      <pubDate>Wed, 25 Sep 2024 21:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Getting-error-0x6985-with-SE05x/m-p/1962055#M1703</guid>
      <dc:creator>ar01</dc:creator>
      <dc:date>2024-09-25T21:47:30Z</dc:date>
    </item>
  </channel>
</rss>