<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NCK2910 PLL Unlock in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/NCK2910-PLL-Unlock/m-p/1961190#M1700</link>
    <description>&lt;P&gt;According to the data manual description，if the temperature change of NCK2910 exceeds 20 ° C, it will trigger the PLL UNLOCK problem.&lt;/P&gt;&lt;P&gt;But we found through temperature box testing that the temperature change at which failure occurs at different starting temperatures is not a stable range of 20 ° C, but rather a range.&lt;/P&gt;&lt;P&gt;We would like to know if there is theoretical calculation support for the relationship between triggering VCO recalibration and temperature when the temperature value exceeds 20 ° C? Or test data？Is there any internal testing data available for NXP to refer to? thank you!&lt;/P&gt;&lt;P&gt;The following table is the data we tested using a temperature box, adjusting the rate of temperature rise and fall to detect temperature changes during the F4 event.&lt;/P&gt;&lt;P&gt;At different starting temperatures, the temperature range for triggering the F4 event is inconsistent, ranging from 21 ℃ to 37 ℃.&lt;/P&gt;&lt;TABLE width="755"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="260.859px" height="62px"&gt;&lt;P&gt;Failure testing----Temperature rise&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="260.859px" height="84px"&gt;&lt;P&gt;time interval（h）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="115.562px" height="84px"&gt;&lt;P&gt;Start Temperature（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="113.078px" height="84px"&gt;&lt;P&gt;Termination temperature（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="135.641px" height="84px"&gt;&lt;P&gt;Temperature difference（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="128.859px" height="84px"&gt;&lt;P&gt;Temperature change rate（℃/min）&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="260.859px" height="40px"&gt;&lt;P&gt;2.6&lt;/P&gt;&lt;/TD&gt;&lt;TD width="115.562px" height="40px"&gt;&lt;P&gt;-19&lt;/P&gt;&lt;/TD&gt;&lt;TD width="113.078px" height="40px"&gt;&lt;P&gt;5&lt;/P&gt;&lt;/TD&gt;&lt;TD width="135.641px" height="40px"&gt;&lt;P&gt;24&lt;/P&gt;&lt;/TD&gt;&lt;TD width="128.859px" height="40px"&gt;&lt;P&gt;0.16&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="260.859px" height="40px"&gt;&lt;P&gt;3.6&lt;/P&gt;&lt;/TD&gt;&lt;TD width="115.562px" height="40px"&gt;&lt;P&gt;5&lt;/P&gt;&lt;/TD&gt;&lt;TD width="113.078px" height="40px"&gt;&lt;P&gt;40&lt;/P&gt;&lt;/TD&gt;&lt;TD width="135.641px" height="40px"&gt;&lt;P&gt;35&lt;/P&gt;&lt;/TD&gt;&lt;TD width="128.859px" height="40px"&gt;&lt;P&gt;0.16&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="260.859px" height="40px"&gt;&lt;P&gt;2.5&lt;/P&gt;&lt;/TD&gt;&lt;TD width="115.562px" height="40px"&gt;&lt;P&gt;27&lt;/P&gt;&lt;/TD&gt;&lt;TD width="113.078px" height="40px"&gt;&lt;P&gt;48&lt;/P&gt;&lt;/TD&gt;&lt;TD width="135.641px" height="40px"&gt;&lt;P&gt;21&lt;/P&gt;&lt;/TD&gt;&lt;TD width="128.859px" height="40px"&gt;&lt;P&gt;0.14&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;TABLE width="755"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="755"&gt;&lt;P&gt;Failure testing-----Temperature drop&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;time interval（h）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;Start Temperature（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;Termination temperature（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;Temperature difference（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;Temperature change rate（℃/min）&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;5.5&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;69&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;34&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;-35&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;0.11&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;3.9&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;52&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;19&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;-33&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;0.14&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;4.0&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;49&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;12&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;-37&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;0.15&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;3.6&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;12&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;-21&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;-33&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;0.15&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;</description>
    <pubDate>Wed, 25 Sep 2024 02:01:59 GMT</pubDate>
    <dc:creator>jiangle</dc:creator>
    <dc:date>2024-09-25T02:01:59Z</dc:date>
    <item>
      <title>NCK2910 PLL Unlock</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/NCK2910-PLL-Unlock/m-p/1961190#M1700</link>
      <description>&lt;P&gt;According to the data manual description，if the temperature change of NCK2910 exceeds 20 ° C, it will trigger the PLL UNLOCK problem.&lt;/P&gt;&lt;P&gt;But we found through temperature box testing that the temperature change at which failure occurs at different starting temperatures is not a stable range of 20 ° C, but rather a range.&lt;/P&gt;&lt;P&gt;We would like to know if there is theoretical calculation support for the relationship between triggering VCO recalibration and temperature when the temperature value exceeds 20 ° C? Or test data？Is there any internal testing data available for NXP to refer to? thank you!&lt;/P&gt;&lt;P&gt;The following table is the data we tested using a temperature box, adjusting the rate of temperature rise and fall to detect temperature changes during the F4 event.&lt;/P&gt;&lt;P&gt;At different starting temperatures, the temperature range for triggering the F4 event is inconsistent, ranging from 21 ℃ to 37 ℃.&lt;/P&gt;&lt;TABLE width="755"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="260.859px" height="62px"&gt;&lt;P&gt;Failure testing----Temperature rise&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="260.859px" height="84px"&gt;&lt;P&gt;time interval（h）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="115.562px" height="84px"&gt;&lt;P&gt;Start Temperature（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="113.078px" height="84px"&gt;&lt;P&gt;Termination temperature（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="135.641px" height="84px"&gt;&lt;P&gt;Temperature difference（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="128.859px" height="84px"&gt;&lt;P&gt;Temperature change rate（℃/min）&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="260.859px" height="40px"&gt;&lt;P&gt;2.6&lt;/P&gt;&lt;/TD&gt;&lt;TD width="115.562px" height="40px"&gt;&lt;P&gt;-19&lt;/P&gt;&lt;/TD&gt;&lt;TD width="113.078px" height="40px"&gt;&lt;P&gt;5&lt;/P&gt;&lt;/TD&gt;&lt;TD width="135.641px" height="40px"&gt;&lt;P&gt;24&lt;/P&gt;&lt;/TD&gt;&lt;TD width="128.859px" height="40px"&gt;&lt;P&gt;0.16&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="260.859px" height="40px"&gt;&lt;P&gt;3.6&lt;/P&gt;&lt;/TD&gt;&lt;TD width="115.562px" height="40px"&gt;&lt;P&gt;5&lt;/P&gt;&lt;/TD&gt;&lt;TD width="113.078px" height="40px"&gt;&lt;P&gt;40&lt;/P&gt;&lt;/TD&gt;&lt;TD width="135.641px" height="40px"&gt;&lt;P&gt;35&lt;/P&gt;&lt;/TD&gt;&lt;TD width="128.859px" height="40px"&gt;&lt;P&gt;0.16&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="260.859px" height="40px"&gt;&lt;P&gt;2.5&lt;/P&gt;&lt;/TD&gt;&lt;TD width="115.562px" height="40px"&gt;&lt;P&gt;27&lt;/P&gt;&lt;/TD&gt;&lt;TD width="113.078px" height="40px"&gt;&lt;P&gt;48&lt;/P&gt;&lt;/TD&gt;&lt;TD width="135.641px" height="40px"&gt;&lt;P&gt;21&lt;/P&gt;&lt;/TD&gt;&lt;TD width="128.859px" height="40px"&gt;&lt;P&gt;0.14&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;TABLE width="755"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="755"&gt;&lt;P&gt;Failure testing-----Temperature drop&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;time interval（h）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;Start Temperature（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;Termination temperature（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;Temperature difference（℃）&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;Temperature change rate（℃/min）&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;5.5&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;69&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;34&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;-35&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;0.11&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;3.9&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;52&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;19&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;-33&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;0.14&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;4.0&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;49&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;12&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;-37&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;0.15&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD width="146"&gt;&lt;P&gt;3.6&lt;/P&gt;&lt;/TD&gt;&lt;TD width="120"&gt;&lt;P&gt;12&lt;/P&gt;&lt;/TD&gt;&lt;TD width="117"&gt;&lt;P&gt;-21&lt;/P&gt;&lt;/TD&gt;&lt;TD width="194"&gt;&lt;P&gt;-33&lt;/P&gt;&lt;/TD&gt;&lt;TD width="177"&gt;&lt;P&gt;0.15&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;</description>
      <pubDate>Wed, 25 Sep 2024 02:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/NCK2910-PLL-Unlock/m-p/1961190#M1700</guid>
      <dc:creator>jiangle</dc:creator>
      <dc:date>2024-09-25T02:01:59Z</dc:date>
    </item>
  </channel>
</rss>