<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic New installation of JCOP Tools gives class file format error in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/New-installation-of-JCOP-Tools-gives-class-file-format-error/m-p/1960957#M1699</link>
    <description>&lt;P&gt;I have a new installation of JCOP Tools which gives "unsupported class file format of version 66.0" error for a basic template applet. This is listed as a known issue in JCOP Tools Getting started app note "If both Eclipse and Java are not same (32 or 64), Following error will be displayed in problem view of Eclipse " however everything is 64-bit.&lt;/P&gt;&lt;P&gt;Java version 22.0.1 (24-04-16)&lt;BR /&gt;JDK version 22&lt;BR /&gt;Eclipse version 4.32.0 (2024-06)&lt;BR /&gt;JCOP Tools version 6.9.0.12&lt;/P&gt;&lt;P&gt;Any suggestions much appreciated.&lt;/P&gt;</description>
    <pubDate>Tue, 24 Sep 2024 17:04:37 GMT</pubDate>
    <dc:creator>markpotts123</dc:creator>
    <dc:date>2024-09-24T17:04:37Z</dc:date>
    <item>
      <title>New installation of JCOP Tools gives class file format error</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/New-installation-of-JCOP-Tools-gives-class-file-format-error/m-p/1960957#M1699</link>
      <description>&lt;P&gt;I have a new installation of JCOP Tools which gives "unsupported class file format of version 66.0" error for a basic template applet. This is listed as a known issue in JCOP Tools Getting started app note "If both Eclipse and Java are not same (32 or 64), Following error will be displayed in problem view of Eclipse " however everything is 64-bit.&lt;/P&gt;&lt;P&gt;Java version 22.0.1 (24-04-16)&lt;BR /&gt;JDK version 22&lt;BR /&gt;Eclipse version 4.32.0 (2024-06)&lt;BR /&gt;JCOP Tools version 6.9.0.12&lt;/P&gt;&lt;P&gt;Any suggestions much appreciated.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Sep 2024 17:04:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/New-installation-of-JCOP-Tools-gives-class-file-format-error/m-p/1960957#M1699</guid>
      <dc:creator>markpotts123</dc:creator>
      <dc:date>2024-09-24T17:04:37Z</dc:date>
    </item>
    <item>
      <title>Re: New installation of JCOP Tools gives class file format error</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/New-installation-of-JCOP-Tools-gives-class-file-format-error/m-p/1988257#M1744</link>
      <description>&lt;P&gt;I was eventually able to resolve this issue, which turned out to be incorrect installation instructions. When installing under Windows the documentation says install Visual C++ Redistributable 2012. This is to ensure critical Windows libraries (DLLs) that the package depends on are present. One of the library dependencies is MFC100.DLL.&lt;/P&gt;&lt;P&gt;However Visual C++ Redistributable 2012 actually installs MFC110.DLL causing a missing library dependency. Installing&amp;nbsp;Visual C++ Redistributable 2010 installs the required MFC100.DLL and JCOP Tools then runs correctly. Hope this is useful to someone else ;-).&lt;/P&gt;</description>
      <pubDate>Tue, 05 Nov 2024 21:50:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/New-installation-of-JCOP-Tools-gives-class-file-format-error/m-p/1988257#M1744</guid>
      <dc:creator>markpotts123</dc:creator>
      <dc:date>2024-11-05T21:50:58Z</dc:date>
    </item>
  </channel>
</rss>