<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Where is jcsim.bat? in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Where-is-jcsim-bat/m-p/1959301#M1698</link>
    <description>&lt;P&gt;I recently obtained access to JCOP Tools and have installed and activated the plugin under Eclipse.&lt;/P&gt;&lt;P&gt;Following the NXP tutorial I started experimenting with JCShell which I was able to successfully load via jcshell.bat from the NXP_JCShell folder.&lt;/P&gt;&lt;P&gt;In order to use the JCOP simulator the tutorial says to first run jcsim.bat however I cannot find this file or the JCOP_Simulation folder shown in the example. Do I have to separately request access to this package?&lt;/P&gt;&lt;P&gt;Any advice appreciated.&lt;BR /&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 22 Sep 2024 19:00:10 GMT</pubDate>
    <dc:creator>markpotts123</dc:creator>
    <dc:date>2024-09-22T19:00:10Z</dc:date>
    <item>
      <title>Where is jcsim.bat?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Where-is-jcsim-bat/m-p/1959301#M1698</link>
      <description>&lt;P&gt;I recently obtained access to JCOP Tools and have installed and activated the plugin under Eclipse.&lt;/P&gt;&lt;P&gt;Following the NXP tutorial I started experimenting with JCShell which I was able to successfully load via jcshell.bat from the NXP_JCShell folder.&lt;/P&gt;&lt;P&gt;In order to use the JCOP simulator the tutorial says to first run jcsim.bat however I cannot find this file or the JCOP_Simulation folder shown in the example. Do I have to separately request access to this package?&lt;/P&gt;&lt;P&gt;Any advice appreciated.&lt;BR /&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 22 Sep 2024 19:00:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Where-is-jcsim-bat/m-p/1959301#M1698</guid>
      <dc:creator>markpotts123</dc:creator>
      <dc:date>2024-09-22T19:00:10Z</dc:date>
    </item>
  </channel>
</rss>