<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: JCOP Shell &amp;quot;Connect to terminal&amp;quot; icon not working in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/JCOP-Shell-quot-Connect-to-terminal-quot-icon-not-working/m-p/1944693#M1672</link>
    <description>&lt;P&gt;Can you use the standalone version of JCShell?&amp;nbsp; I'd try installing that and making sure it runs.&amp;nbsp; If it does, it's a probably a problem specific to Eclipse, otherwise it's probably a problem with Eclipse.&lt;/P&gt;&lt;P&gt;I seem to remember having some issues with the most recent versions of Eclipse having their own copy of the Java runtime in them.&amp;nbsp;&amp;nbsp; There were a few ENV vars that weren't set quite properly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Basically, I think you may need to have JAVA_HOME set as part of the eclipse.ini:&lt;/P&gt;&lt;P&gt;-DJAVA_HOME=C:/Users/xxxx/.p2/pool/plugins/org.eclipse.justj.openjdk.hotspot.jre.full.win32.x86_64_17.0.7.v20230425-1502/jre&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 30 Aug 2024 19:52:45 GMT</pubDate>
    <dc:creator>msjcard</dc:creator>
    <dc:date>2024-08-30T19:52:45Z</dc:date>
    <item>
      <title>JCOP Shell "Connect to terminal" icon not working</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/JCOP-Shell-quot-Connect-to-terminal-quot-icon-not-working/m-p/1931235#M1658</link>
      <description>&lt;P&gt;I recently installed Java 17 and after that the "Connect to terminal" icon in the JCOP Shell within Eclipse no longer worked. I installed another version of Eclipse and re-installed the JCOP tools, but the icon still does not work.&lt;/P&gt;&lt;P&gt;I have the following installed:&lt;/P&gt;&lt;P&gt;Eclipse IDE, version 2020-09, Build id: 20200910-1200&lt;/P&gt;&lt;P&gt;NXP JCOP Tools 6.9.0.12&amp;nbsp; - com.nxp.id.jcop.eclipse&lt;/P&gt;&lt;P&gt;NXP Target-Pack for NXP JCOP Tools&amp;nbsp; 6.9.0.12 - com.nxp.id.jcop.eclipse.targetpacks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Aug 2024 15:41:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/JCOP-Shell-quot-Connect-to-terminal-quot-icon-not-working/m-p/1931235#M1658</guid>
      <dc:creator>Jim_Coon</dc:creator>
      <dc:date>2024-08-13T15:41:06Z</dc:date>
    </item>
    <item>
      <title>Re: JCOP Shell "Connect to terminal" icon not working</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/JCOP-Shell-quot-Connect-to-terminal-quot-icon-not-working/m-p/1944693#M1672</link>
      <description>&lt;P&gt;Can you use the standalone version of JCShell?&amp;nbsp; I'd try installing that and making sure it runs.&amp;nbsp; If it does, it's a probably a problem specific to Eclipse, otherwise it's probably a problem with Eclipse.&lt;/P&gt;&lt;P&gt;I seem to remember having some issues with the most recent versions of Eclipse having their own copy of the Java runtime in them.&amp;nbsp;&amp;nbsp; There were a few ENV vars that weren't set quite properly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Basically, I think you may need to have JAVA_HOME set as part of the eclipse.ini:&lt;/P&gt;&lt;P&gt;-DJAVA_HOME=C:/Users/xxxx/.p2/pool/plugins/org.eclipse.justj.openjdk.hotspot.jre.full.win32.x86_64_17.0.7.v20230425-1502/jre&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Aug 2024 19:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/JCOP-Shell-quot-Connect-to-terminal-quot-icon-not-working/m-p/1944693#M1672</guid>
      <dc:creator>msjcard</dc:creator>
      <dc:date>2024-08-30T19:52:45Z</dc:date>
    </item>
  </channel>
</rss>