<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックHow can I do write and read as secure data or keys</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/How-can-I-do-write-and-read-as-secure-data-or-keys/m-p/1825763#M1548</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Does SE050 support writing and reading private keys?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to write and read binary more than 8k?&amp;nbsp;&lt;BR /&gt;The APIsSe05x_API_WriteBinary/Se05x_API_ReadObject allow me to do up to 8k,&lt;BR /&gt;but the SE050 datasheet specifies 50k secure data or keys. Could you tell me how I can use other memory for writing and reading?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Sureshkumar R&lt;/P&gt;</description>
    <pubDate>Tue, 12 Mar 2024 05:30:35 GMT</pubDate>
    <dc:creator>krsuresh</dc:creator>
    <dc:date>2024-03-12T05:30:35Z</dc:date>
    <item>
      <title>How can I do write and read as secure data or keys</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/How-can-I-do-write-and-read-as-secure-data-or-keys/m-p/1825763#M1548</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Does SE050 support writing and reading private keys?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to write and read binary more than 8k?&amp;nbsp;&lt;BR /&gt;The APIsSe05x_API_WriteBinary/Se05x_API_ReadObject allow me to do up to 8k,&lt;BR /&gt;but the SE050 datasheet specifies 50k secure data or keys. Could you tell me how I can use other memory for writing and reading?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Sureshkumar R&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 05:30:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/How-can-I-do-write-and-read-as-secure-data-or-keys/m-p/1825763#M1548</guid>
      <dc:creator>krsuresh</dc:creator>
      <dc:date>2024-03-12T05:30:35Z</dc:date>
    </item>
    <item>
      <title>Re: How can I do write and read as secure data or keys</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/How-can-I-do-write-and-read-as-secure-data-or-keys/m-p/1825818#M1550</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210184"&gt;@krsuresh&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;SE05x supports writing private key into this device if the policy of the key object allows, but not possible to read the private key out of the device.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The bin file length can reach up to 0x7FFF but also limited by the free space left in the device when you create this bin file.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The APDU commands can be used to create/write or read the secure objects in the device, but for application purpose, I would recommend the SSS APIs out of the Plug&amp;amp;Trust MW. You may refer to the demo of ex_ecc or ex_rsa for more details.&lt;/P&gt;
&lt;P&gt;Please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-and-trust-secure-element-family-enhanced-iot-security-with-high-flexibility:SE050" target="_blank"&gt;https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-and-trust-secure-element-family-enhanced-iot-security-with-high-flexibility:SE050&lt;/A&gt;&amp;nbsp;for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 06:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/How-can-I-do-write-and-read-as-secure-data-or-keys/m-p/1825818#M1550</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-03-12T06:53:40Z</dc:date>
    </item>
  </channel>
</rss>