<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure Authentication中的主题 Re: SE050 library optimization</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-library-optimization/m-p/1789228#M1501</link>
    <description>&lt;P&gt;How can i include inside mi full Plug &amp;amp; Trust Middleware project started from the SDK demo on Windows?&lt;/P&gt;&lt;P&gt;There's any application note avaibile?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jan 2024 07:37:11 GMT</pubDate>
    <dc:creator>WorkerEmbedded</dc:creator>
    <dc:date>2024-01-16T07:37:11Z</dc:date>
    <item>
      <title>SE050 library optimization</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-library-optimization/m-p/1788718#M1497</link>
      <description>&lt;P&gt;Hi everybody!&lt;/P&gt;&lt;P&gt;I've got just a little question about SE050 library and how can i optimize it.&lt;/P&gt;&lt;P&gt;My goal is to flash a project developed on LPC55S69 (it's like 610 Kb) inside another LPC55 with a 64 Kb dataflash.&lt;/P&gt;&lt;P&gt;My project was develop starting from a SE05X demo and now it's about 270 Kb.&lt;/P&gt;&lt;P&gt;The library is very heavy, there's a way to reduce it without disable important config like ECC and AES calulation (iniside the fsl_sss_ftr.h).&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jan 2024 10:16:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-library-optimization/m-p/1788718#M1497</guid>
      <dc:creator>WorkerEmbedded</dc:creator>
      <dc:date>2024-01-15T10:16:56Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 library optimization</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-library-optimization/m-p/1789058#M1498</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224071"&gt;@WorkerEmbedded&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The nano package of MW should meet your requirements, please kindly refer to&amp;nbsp;&lt;A href="https://github.com/NXPPlugNTrust/nano-package/tree/master" target="_blank"&gt;https://github.com/NXPPlugNTrust/nano-package/tree/master&lt;/A&gt;&amp;nbsp;for details.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jan 2024 02:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-library-optimization/m-p/1789058#M1498</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-01-16T02:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 library optimization</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-library-optimization/m-p/1789228#M1501</link>
      <description>&lt;P&gt;How can i include inside mi full Plug &amp;amp; Trust Middleware project started from the SDK demo on Windows?&lt;/P&gt;&lt;P&gt;There's any application note avaibile?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jan 2024 07:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-library-optimization/m-p/1789228#M1501</guid>
      <dc:creator>WorkerEmbedded</dc:creator>
      <dc:date>2024-01-16T07:37:11Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 library optimization</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-library-optimization/m-p/1789922#M1502</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224071"&gt;@WorkerEmbedded&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The nano package doesn't support SSS APIs, so if your application is based on SSS APIs, you have to refine it with SE05X APIs instead.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 03:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-library-optimization/m-p/1789922#M1502</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-01-17T03:43:58Z</dc:date>
    </item>
  </channel>
</rss>