<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: SE05x-PLUG-TRUST-MW version 04.05.00 is missing PSA.proto</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1782876#M1480</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223506"&gt;@stefanct&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The PSA.proto file is used just in case of RW61x target which is not yet supported in P&amp;amp;T MW release; for this reason the PSA.proto file is excluded.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Jan 2024 09:03:16 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2024-01-04T09:03:16Z</dc:date>
    <item>
      <title>SE05x-PLUG-TRUST-MW version 04.05.00 is missing PSA.proto</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1779474#M1469</link>
      <description>&lt;P&gt;nxp_iot_agent/doc/protobuf/Dispatcher.proto is importing PSA.proto which is not contained in the archive.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Dec 2023 00:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1779474#M1469</guid>
      <dc:creator>stefanct</dc:creator>
      <dc:date>2023-12-25T00:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: SE05x-PLUG-TRUST-MW version 04.05.00 is missing PSA.proto</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1782876#M1480</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223506"&gt;@stefanct&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The PSA.proto file is used just in case of RW61x target which is not yet supported in P&amp;amp;T MW release; for this reason the PSA.proto file is excluded.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jan 2024 09:03:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1782876#M1480</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-01-04T09:03:16Z</dc:date>
    </item>
    <item>
      <title>Re: SE05x-PLUG-TRUST-MW version 04.05.00 is missing PSA.proto</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1784402#M1483</link>
      <description>It breaks execution of 'semslite_json_converter.py . protoc'. If it's not included it should not be referenced in Dispatcher.proto</description>
      <pubDate>Mon, 08 Jan 2024 11:24:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1784402#M1483</guid>
      <dc:creator>stefanct</dc:creator>
      <dc:date>2024-01-08T11:24:26Z</dc:date>
    </item>
    <item>
      <title>Re: SE05x-PLUG-TRUST-MW version 04.05.00 is missing PSA.proto</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1784997#M1486</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223506"&gt;@stefanct&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have you tried to comment the reference out in&amp;nbsp;&lt;SPAN&gt;Dispatcher.proto? Does it work for your case?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jan 2024 07:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1784997#M1486</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-01-09T07:49:36Z</dc:date>
    </item>
    <item>
      <title>Re: SE05x-PLUG-TRUST-MW version 04.05.00 is missing PSA.proto</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1785299#M1487</link>
      <description>&lt;P&gt;Yes, of course. The PSA definitions are used in two places that have to be disabled as well, see attachment.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jan 2024 13:55:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE05x-PLUG-TRUST-MW-version-04-05-00-is-missing-PSA-proto/m-p/1785299#M1487</guid>
      <dc:creator>stefanct</dc:creator>
      <dc:date>2024-01-09T13:55:15Z</dc:date>
    </item>
  </channel>
</rss>