<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SE05x as secure (data) vault for end user in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE05x-as-secure-data-vault-for-end-user/m-p/1758172#M1443</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196615"&gt;@frix&lt;/a&gt;&amp;nbsp;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, SE050E meets your requirements.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 16 Nov 2023 07:47:27 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2023-11-16T07:47:27Z</dc:date>
    <item>
      <title>SE05x as secure (data) vault for end user</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE05x-as-secure-data-vault-for-end-user/m-p/1756465#M1439</link>
      <description>&lt;P&gt;Good day,&lt;/P&gt;&lt;P&gt;I'm evaluating the SE050E to see if it can be used to store end user data (keys) securely. For proof of concept I'd like to use a Raspberry PI, which connects over USB to an external device (PC).&amp;nbsp;The SE050E devkit is attached to the Raspberry PI.&lt;/P&gt;&lt;P&gt;An application running on the Raspberry PI will interpret the commands from the PC and perform the necessary tasks on the SE050.&lt;/P&gt;&lt;P&gt;A new UserID needs to be created, with limited authentication attempts (5), from the PC. The end user of the system provides their own PIN.&lt;/P&gt;&lt;P&gt;To use the system the end user must provide their PIN to unlock the UserID profile.&lt;/P&gt;&lt;P&gt;If the authentication attempts are exceeded the UserID is locked permanently.&lt;/P&gt;&lt;P&gt;If&amp;nbsp;RESERVED_ID_FACTORY_RESET was set during the creation of the UserID, the external application, running on the Raspberry PI, is able to delete the account.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please confirm if the SE050E will meet the use case requirement:&lt;/P&gt;&lt;P&gt;-- Create new UserID,&lt;/P&gt;&lt;P&gt;-- UserID is inaccessible / disabled after authentication attempt limit was reached&lt;/P&gt;&lt;P&gt;-- Delete (locked) UserID (without knowing the PIN)&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Frix&lt;/P&gt;</description>
      <pubDate>Mon, 13 Nov 2023 19:15:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE05x-as-secure-data-vault-for-end-user/m-p/1756465#M1439</guid>
      <dc:creator>frix</dc:creator>
      <dc:date>2023-11-13T19:15:52Z</dc:date>
    </item>
    <item>
      <title>Re: SE05x as secure (data) vault for end user</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE05x-as-secure-data-vault-for-end-user/m-p/1758172#M1443</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196615"&gt;@frix&lt;/a&gt;&amp;nbsp;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, SE050E meets your requirements.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 07:47:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE05x-as-secure-data-vault-for-end-user/m-p/1758172#M1443</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-11-16T07:47:27Z</dc:date>
    </item>
  </channel>
</rss>