<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Does the EdgeLock SE050 applet support sensor data protection? in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Does-the-EdgeLock-SE050-applet-support-sensor-data-protection/m-p/980885#M142</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it does. The EdgeLock SE050 allows you to set up a secure, end-to-end connection from the&lt;BR /&gt;sensor or actuator to your local IoT gateway or cloud-based service, protecting the&lt;BR /&gt;interface between the sensor and the security IC. As such, EdgeLock SE050 helps you to&lt;BR /&gt;provide a higher level of security in your IoT system by:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Preventing data manipulation: The data extracted by the sensor is collected privately&lt;BR /&gt;and cannot be manipulated.&lt;/LI&gt;&lt;LI&gt;Authenticating the sensor: The system authenticates the sensor as a proof of origin.&lt;/LI&gt;&lt;LI&gt;Providing end-to-end security: The data collected over the private sensor can be&lt;BR /&gt;encrypted and securely transferred to your gateway or cloud for further treatment and&lt;BR /&gt;analysis.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;For more information, you can refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN12449.pdf"&gt;AN12449- Sensor data protection with EdgeLock SE050&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Oct 2019 14:24:34 GMT</pubDate>
    <dc:creator>jordijofrenxp</dc:creator>
    <dc:date>2019-10-29T14:24:34Z</dc:date>
    <item>
      <title>Does the EdgeLock SE050 applet support sensor data protection?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Does-the-EdgeLock-SE050-applet-support-sensor-data-protection/m-p/980885#M142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it does. The EdgeLock SE050 allows you to set up a secure, end-to-end connection from the&lt;BR /&gt;sensor or actuator to your local IoT gateway or cloud-based service, protecting the&lt;BR /&gt;interface between the sensor and the security IC. As such, EdgeLock SE050 helps you to&lt;BR /&gt;provide a higher level of security in your IoT system by:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Preventing data manipulation: The data extracted by the sensor is collected privately&lt;BR /&gt;and cannot be manipulated.&lt;/LI&gt;&lt;LI&gt;Authenticating the sensor: The system authenticates the sensor as a proof of origin.&lt;/LI&gt;&lt;LI&gt;Providing end-to-end security: The data collected over the private sensor can be&lt;BR /&gt;encrypted and securely transferred to your gateway or cloud for further treatment and&lt;BR /&gt;analysis.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;For more information, you can refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN12449.pdf"&gt;AN12449- Sensor data protection with EdgeLock SE050&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2019 14:24:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Does-the-EdgeLock-SE050-applet-support-sensor-data-protection/m-p/980885#M142</guid>
      <dc:creator>jordijofrenxp</dc:creator>
      <dc:date>2019-10-29T14:24:34Z</dc:date>
    </item>
  </channel>
</rss>