<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: SE050F2 as Smart card interface</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1738126#M1378</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219018"&gt;@hitesh_gambhava&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Not sure what is the requirement meant when you specified "smart card interface". SE050F is a "smart card". It can receive commands using the interfaces I²C (using T1oI2C protocol), and ISO14443. When you place the NFC antenna over a contactless reader, it will be discovered as a smart card. The contact based ISO7816 interface is a classic smart card interface, but it does not matter of the commands are exchanges over contact, contactless or I2C interface. Over all interfaces the SE05x can be made recognized by an system as "smart card". E.g. for the I2C interface the K64F CCID example can be used which shows the connected SE05x as a smart card to a host system. Most likely your question is if the SE050F then supports the commands expected by the system, right? Please kindly clarify.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 12 Oct 2023 02:35:09 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2023-10-12T02:35:09Z</dc:date>
    <item>
      <title>SE050F2 as Smart card interface</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1736583#M1376</link>
      <description>&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;I have a query with SE050F2 secure element. Can it work as smart card over I2C interface or it is must to use ISO 7816 to get this functionality?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hitesh&lt;/P&gt;</description>
      <pubDate>Tue, 10 Oct 2023 12:52:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1736583#M1376</guid>
      <dc:creator>hitesh_gambhava</dc:creator>
      <dc:date>2023-10-10T12:52:36Z</dc:date>
    </item>
    <item>
      <title>Re: SE050F2 as Smart card interface</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1738126#M1378</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219018"&gt;@hitesh_gambhava&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Not sure what is the requirement meant when you specified "smart card interface". SE050F is a "smart card". It can receive commands using the interfaces I²C (using T1oI2C protocol), and ISO14443. When you place the NFC antenna over a contactless reader, it will be discovered as a smart card. The contact based ISO7816 interface is a classic smart card interface, but it does not matter of the commands are exchanges over contact, contactless or I2C interface. Over all interfaces the SE05x can be made recognized by an system as "smart card". E.g. for the I2C interface the K64F CCID example can be used which shows the connected SE05x as a smart card to a host system. Most likely your question is if the SE050F then supports the commands expected by the system, right? Please kindly clarify.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 02:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1738126#M1378</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-10-12T02:35:09Z</dc:date>
    </item>
    <item>
      <title>Re: SE050F2 as Smart card interface</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1739963#M1384</link>
      <description>&lt;P&gt;Hi Kan,&lt;/P&gt;&lt;P&gt;Thanks for the response. My question is more about as classic Smart card interface i.e. from PC/Laptop USB to K64F USB (over CCID) and K64F to SE050 over I2C interface. As per your response it looks this is possible. Please confirm.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hitesh&lt;/P&gt;</description>
      <pubDate>Mon, 16 Oct 2023 04:16:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1739963#M1384</guid>
      <dc:creator>hitesh_gambhava</dc:creator>
      <dc:date>2023-10-16T04:16:02Z</dc:date>
    </item>
    <item>
      <title>Re: SE050F2 as Smart card interface</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1740043#M1385</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219018"&gt;@hitesh_gambhava&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, you may use either of the following CCID examples out of the MW for evaluation purpose.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_1-1697435820985.png" style="width: 650px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/245176i9CBDB2606131579B/image-dimensions/650x91?v=v2" width="650" height="91" role="button" title="Kan_Li_1-1697435820985.png" alt="Kan_Li_1-1697435820985.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;and after plugging into a Laptop, you will find the following notification.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1697435774825.png" style="width: 512px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/245175iE8164F35681211CD/image-dimensions/512x168?v=v2" width="512" height="168" role="button" title="Kan_Li_0-1697435774825.png" alt="Kan_Li_0-1697435774825.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regarding how to program the bin file into the K64F-FRDM board, please kindly refer to "3.3 Flash FRDM-K64F with VCOM software " in&amp;nbsp;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12398.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12398.pdf&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 16 Oct 2023 06:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1740043#M1385</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-10-16T06:02:35Z</dc:date>
    </item>
    <item>
      <title>Re: SE050F2 as Smart card interface</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1740154#M1387</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for the confirmation. Yes, this information will really help for further development.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hitesh&lt;/P&gt;</description>
      <pubDate>Mon, 16 Oct 2023 07:43:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050F2-as-Smart-card-interface/m-p/1740154#M1387</guid>
      <dc:creator>hitesh_gambhava</dc:creator>
      <dc:date>2023-10-16T07:43:45Z</dc:date>
    </item>
  </channel>
</rss>