<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure Authentication中的主题 SE050 - How access an inject certificate using openssl</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-How-access-an-inject-certificate-using-openssl/m-p/1702012#M1332</link>
    <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I am able to inject an RSA certificate into the SE &lt;SPAN&gt;with success&lt;/SPAN&gt;.&lt;BR /&gt;But now I need to use my certificate through an openssl command.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know that it is possible, using openssl, to access an element through the "-key refkeyfile.ref" command.&lt;BR /&gt;But if I understood correctly the concept of a reference key, it is a reference to the private key, and not to an element, that is, if my element is a certificate or a public key, I am not able to generate a reference key.&lt;/P&gt;&lt;P&gt;How can I access an injected certificate from an openssl command without the reference key?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Cristiane Bellenzier Piaia&lt;/P&gt;</description>
    <pubDate>Wed, 09 Aug 2023 13:58:39 GMT</pubDate>
    <dc:creator>CristianeBP</dc:creator>
    <dc:date>2023-08-09T13:58:39Z</dc:date>
    <item>
      <title>SE050 - How access an inject certificate using openssl</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-How-access-an-inject-certificate-using-openssl/m-p/1702012#M1332</link>
      <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I am able to inject an RSA certificate into the SE &lt;SPAN&gt;with success&lt;/SPAN&gt;.&lt;BR /&gt;But now I need to use my certificate through an openssl command.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know that it is possible, using openssl, to access an element through the "-key refkeyfile.ref" command.&lt;BR /&gt;But if I understood correctly the concept of a reference key, it is a reference to the private key, and not to an element, that is, if my element is a certificate or a public key, I am not able to generate a reference key.&lt;/P&gt;&lt;P&gt;How can I access an injected certificate from an openssl command without the reference key?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Cristiane Bellenzier Piaia&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 13:58:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-How-access-an-inject-certificate-using-openssl/m-p/1702012#M1332</guid>
      <dc:creator>CristianeBP</dc:creator>
      <dc:date>2023-08-09T13:58:39Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 - How access an inject certificate using openssl</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-How-access-an-inject-certificate-using-openssl/m-p/1702530#M1333</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221468"&gt;@CristianeBP&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may use a tool like ssscli to get the injected cert from the SE and store it in the native file system, then it can accessed by the openssl command.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1691632827321.png" style="width: 628px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/235873i2D3176CDF56EE0BE/image-dimensions/628x256?v=v2" width="628" height="256" role="button" title="Kan_Li_0-1691632827321.png" alt="Kan_Li_0-1691632827321.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please kindly refer to "simw-top/doc/pycli/doc/cli_commands_list.html" for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 10 Aug 2023 02:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-How-access-an-inject-certificate-using-openssl/m-p/1702530#M1333</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-08-10T02:01:34Z</dc:date>
    </item>
  </channel>
</rss>