<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: SCP03 default keys</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SCP03-default-keys/m-p/1699769#M1329</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/150525"&gt;@deang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, there is some OEF ID info issue in table 6, please refer to table 2 instead, alternatively you may refer to the mapping info you found in&amp;nbsp;&lt;SPAN&gt;the PlugTrust library (ex_sss_tp_scp03_keys.h). The update for AN12436 is in progress, I will let you know when it is available.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Mon, 07 Aug 2023 02:01:29 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2023-08-07T02:01:29Z</dc:date>
    <item>
      <title>SCP03 default keys</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SCP03-default-keys/m-p/1699563#M1328</link>
      <description>&lt;P&gt;The default SCP03 keys listed in:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12436.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12436.pdf&lt;/A&gt;&amp;nbsp; are incorrect.&amp;nbsp; The following is a code snippet from the PlugTrust library (ex_sss_tp_scp03_keys.h):&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;// Variant ==&amp;gt; OEF ID&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;// SE050A1 ==&amp;gt; A204&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;// SE050A2 ==&amp;gt; A205&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;// SE050B1 ==&amp;gt; A202&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;// SE050B2 ==&amp;gt; A203&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;// SE050C1 ==&amp;gt; A200&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;// SE050C2 ==&amp;gt; A201&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;// Development Board ==&amp;gt; A1F4 (DEVKIT)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;//SE051C ==&amp;gt;0xA8FA&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;//SE051A ==&amp;gt;0xA920&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;//SE050E ==&amp;gt;0xA921&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;//SE051W(Fira) ==&amp;gt;0xA739&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;//A5000 gen ==&amp;gt;0xA736&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;//SE050F2 ==&amp;gt;0xA92A&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Are these mappings correct?&lt;/P&gt;&lt;P&gt;Also when will the AN12436 app note be updated?&lt;/P&gt;&lt;P&gt;Dean&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Aug 2023 18:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SCP03-default-keys/m-p/1699563#M1328</guid>
      <dc:creator>deang</dc:creator>
      <dc:date>2023-08-04T18:56:13Z</dc:date>
    </item>
    <item>
      <title>Re: SCP03 default keys</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SCP03-default-keys/m-p/1699769#M1329</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/150525"&gt;@deang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, there is some OEF ID info issue in table 6, please refer to table 2 instead, alternatively you may refer to the mapping info you found in&amp;nbsp;&lt;SPAN&gt;the PlugTrust library (ex_sss_tp_scp03_keys.h). The update for AN12436 is in progress, I will let you know when it is available.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 02:01:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SCP03-default-keys/m-p/1699769#M1329</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-08-07T02:01:29Z</dc:date>
    </item>
    <item>
      <title>Re: SCP03 default keys</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SCP03-default-keys/m-p/1700299#M1330</link>
      <description>&lt;P&gt;Thanks Kan.&lt;/P&gt;&lt;P&gt;I double checked and I've got all of the variants and correct keys set in my code. For ease of refence, here's the list of OEFIDs and variants.&lt;/P&gt;&lt;P&gt;A201 == SE050C2&lt;BR /&gt;A200 == SE050C1&lt;BR /&gt;A921 == SE050E2&lt;BR /&gt;A92A == SE050F2&lt;BR /&gt;A204 == SE050A1&lt;BR /&gt;A205 == SE050A2&lt;BR /&gt;A43B == SE050D2&lt;BR /&gt;A202 == SE050B1&lt;BR /&gt;A203 == SE050B2&lt;BR /&gt;A77E == SE050F2&lt;/P&gt;&lt;P&gt;Dean&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 14:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SCP03-default-keys/m-p/1700299#M1330</guid>
      <dc:creator>deang</dc:creator>
      <dc:date>2023-08-07T14:44:52Z</dc:date>
    </item>
  </channel>
</rss>