<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: Reading RESERVED_ID_UNIQUE_ID</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Reading-RESERVED-ID-UNIQUE-ID/m-p/1698016#M1326</link>
    <description>&lt;P&gt;Hi Kan,&lt;/P&gt;&lt;P&gt;Thanks for the help.&amp;nbsp; Using the exact size (18 bytes) fixed the problem. I do think the Se05x_API_ReadObject() should allow for a larger than necessary buffer vs. the exact size.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dean&lt;/P&gt;</description>
    <pubDate>Wed, 02 Aug 2023 20:17:45 GMT</pubDate>
    <dc:creator>deang</dc:creator>
    <dc:date>2023-08-02T20:17:45Z</dc:date>
    <item>
      <title>Reading RESERVED_ID_UNIQUE_ID</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Reading-RESERVED-ID-UNIQUE-ID/m-p/1697004#M1323</link>
      <description>&lt;P&gt;1. Are there any special requirements for reading the unique ID?&amp;nbsp; Specifically the&amp;nbsp;RESERVED_ID_UNIQUE_ID?&amp;nbsp; I am connected using a plain connection, the error I keep running into is&amp;nbsp;SM_ERR_CONDITIONS_OF_USE_NOT_SATISFIED.&amp;nbsp; Do I need to be connect via SCP03?&lt;/P&gt;&lt;P&gt;2. What is the size of this data?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dean&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 00:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Reading-RESERVED-ID-UNIQUE-ID/m-p/1697004#M1323</guid>
      <dc:creator>deang</dc:creator>
      <dc:date>2023-08-02T00:40:12Z</dc:date>
    </item>
    <item>
      <title>Re: Reading RESERVED_ID_UNIQUE_ID</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Reading-RESERVED-ID-UNIQUE-ID/m-p/1697134#M1324</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/150525"&gt;@deang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No specific requirement to read this object, we provide a code snippet in nxp_iot_agent_demo for that purpose, please kindly refer to the following for more details.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1690947142749.png" style="width: 677px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/234648i8AA8B691CA0F4BBB/image-dimensions/677x376?v=v2" width="677" height="376" role="button" title="Kan_Li_0-1690947142749.png" alt="Kan_Li_0-1690947142749.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Kan_Li_0-1690947142749.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 03:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Reading-RESERVED-ID-UNIQUE-ID/m-p/1697134#M1324</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-08-02T03:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: Reading RESERVED_ID_UNIQUE_ID</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Reading-RESERVED-ID-UNIQUE-ID/m-p/1698016#M1326</link>
      <description>&lt;P&gt;Hi Kan,&lt;/P&gt;&lt;P&gt;Thanks for the help.&amp;nbsp; Using the exact size (18 bytes) fixed the problem. I do think the Se05x_API_ReadObject() should allow for a larger than necessary buffer vs. the exact size.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dean&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 20:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Reading-RESERVED-ID-UNIQUE-ID/m-p/1698016#M1326</guid>
      <dc:creator>deang</dc:creator>
      <dc:date>2023-08-02T20:17:45Z</dc:date>
    </item>
  </channel>
</rss>