<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: Does the Edge Lock SE050 Plug &amp;amp; Trust middleware support non NXP MCU / MPU boards?</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Does-the-EdgeLock-SE050-Plug-Trust-middleware-support-non-NXP/m-p/1686723#M1305</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;this is the new NXP weblink of this application note (old link does not work anymore).&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;&lt;A title="https://www.nxp.com/docs/en/application-note/an12448.pdf" href="https://www.nxp.com/docs/en/application-note/AN12448.pdf" target="_blank" rel="noreferrer noopener"&gt;https://www.nxp.com/docs/en/application-note/AN12448.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Cheers&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Rodolfo&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jul 2023 14:16:51 GMT</pubDate>
    <dc:creator>rodolfoveltrigo</dc:creator>
    <dc:date>2023-07-12T14:16:51Z</dc:date>
    <item>
      <title>Does the EdgeLock SE050 Plug &amp; Trust middleware support non NXP MCU / MPU boards?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Does-the-EdgeLock-SE050-Plug-Trust-middleware-support-non-NXP/m-p/981083#M146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The EdgeLock SE050 Plug &amp;amp; Trust middleware comes with pre-built support for many NXP MCU / MPU boards. However, you can also leverage SE050 Plug &amp;amp; Trust middleware if you are using any other MCU / MPU board. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From an HW perspective, you can use the OM-SE050ARD evaluation board to connect your board via the Arduino connectors or the external I2C connector. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From an SW perspective, The EdgeLock SE050 Plug &amp;amp; Trust middleware has been designed to facilitate portability to multiple platforms and OS. For more information about how to port the middleware, you can refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN12488-SE050_middleware_porting_guidelines.pdf"&gt;AN12448 SE050 Plug &amp;amp; Trust middleware porting guidelines&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2019 14:26:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Does-the-EdgeLock-SE050-Plug-Trust-middleware-support-non-NXP/m-p/981083#M146</guid>
      <dc:creator>jordijofrenxp</dc:creator>
      <dc:date>2019-10-29T14:26:52Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Edge Lock SE050 Plug &amp; Trust middleware support non NXP MCU / MPU boards?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Does-the-EdgeLock-SE050-Plug-Trust-middleware-support-non-NXP/m-p/1686723#M1305</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;this is the new NXP weblink of this application note (old link does not work anymore).&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;&lt;A title="https://www.nxp.com/docs/en/application-note/an12448.pdf" href="https://www.nxp.com/docs/en/application-note/AN12448.pdf" target="_blank" rel="noreferrer noopener"&gt;https://www.nxp.com/docs/en/application-note/AN12448.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Cheers&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Rodolfo&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 14:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Does-the-EdgeLock-SE050-Plug-Trust-middleware-support-non-NXP/m-p/1686723#M1305</guid>
      <dc:creator>rodolfoveltrigo</dc:creator>
      <dc:date>2023-07-12T14:16:51Z</dc:date>
    </item>
  </channel>
</rss>