<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure Authentication中的主题 Re: Yocto recipe for SE050x</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/975253#M124</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the sharing!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Mar 2020 05:10:21 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2020-03-05T05:10:21Z</dc:date>
    <item>
      <title>Yocto recipe for SE050x</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/975251#M122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to create a recipe to add se050x libraries to my yocto image for imx8 but without success...&lt;/P&gt;&lt;P&gt;Can you provide the recipe used in SD Card image for imx6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_compile&lt;BR /&gt;| INFO:__main__:Preprocessing /home/antonio/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/se050x/1.0-r0/simw-top/ext/open62541/tools/schema/Opc.Ua.NodeSet2.Minimal.xml&lt;BR /&gt;| INFO:__main__:Generating Code for Backend: open62541&lt;BR /&gt;| INFO:__main__:NodeSet generation code successfully printed&lt;BR /&gt;| -- BUILD_TYPE: Debug&lt;BR /&gt;| Found: /home/antonio/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/se050x/1.0-r0/recipe-sysroot-native/usr/lib/libssl.so/home/antonio/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/se050x/1.0-r0/recipe-sysroot-native/usr/lib/libcrypto.so&lt;BR /&gt;| -- CMAKE_CXX_COMPILER_ID = GNU&lt;BR /&gt;| -- CMAKE_SYSTEM_NAME = Linux&lt;BR /&gt;| -- Configuring done&lt;BR /&gt;| -- Generating done&lt;BR /&gt;| -- Build files have been written to: /home/antonio/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/se050x/1.0-r0/simw-top_build/imx_native_a7x_sci2c&lt;BR /&gt;| -- BUILD_TYPE: Debug&lt;BR /&gt;| Found: /home/antonio/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/se050x/1.0-r0/recipe-sysroot-native/usr/lib/libssl.so/home/antonio/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/se050x/1.0-r0/recipe-sysroot-native/usr/lib/libcrypto.so&lt;BR /&gt;| -- CMAKE_CXX_COMPILER_ID = GNU&lt;BR /&gt;| -- CMAKE_SYSTEM_NAME = Linux&lt;BR /&gt;| -- SE05X_Auth - UserID&lt;BR /&gt;| -- se05x_Delete_and_test_provision is not built because SE05X_Auth is 'UserID'.&lt;BR /&gt;| -- Configuring done&lt;BR /&gt;| -- Generating done&lt;BR /&gt;| -- Build files have been written to: /home/antonio/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/se050x/1.0-r0/simw-top_build/imx_native_se050_t1oi2c&lt;BR /&gt;| &lt;BR /&gt;| &lt;BR /&gt;| ### Native compilation on iMX Linux for A71CH using SCI2C&lt;BR /&gt;| #cmake -DSE05X_Auth=None -DSMCOM=SCI2C -DHostCrypto=OPENSSL -DApplet=A71CH -DHost=iMXLinux -DCMAKE_BUILD_TYPE=Debug&lt;BR /&gt;| &lt;BR /&gt;| &lt;BR /&gt;| ### Native compilation on iMX Linux for SE05X using T=1 Over I2C&lt;BR /&gt;| #cmake -DSE05X_Auth=UserID -DSMCOM=T1oI2C -DHostCrypto=OPENSSL -DApplet=SE050_C -DHost=iMXLinux -DCMAKE_BUILD_TYPE=Debug&lt;BR /&gt;| NOTE: make -j 8&lt;BR /&gt;| [ 12%] Built target smCom&lt;BR /&gt;| [ 13%] Linking C executable ../../../bin/jrcpv1_server&lt;BR /&gt;| [ 17%] Built target unity&lt;BR /&gt;| [ 21%] Built target se05x&lt;BR /&gt;| [ 26%] Built target a7x_utils&lt;BR /&gt;| /home/antonio/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/se050x/1.0-r0/recipe-sysroot-native/usr/lib/libssl.so: error adding symbols: File in wrong format&lt;BR /&gt;| collect2: error: ld returned 1 exit status&lt;BR /&gt;| hostlib/hostLib/rjct/CMakeFiles/jrcpv1_server.dir/build.make:149: recipe for target 'bin/jrcpv1_server' failed&lt;BR /&gt;| make[2]: *** [bin/jrcpv1_server] Error 1&lt;BR /&gt;| CMakeFiles/Makefile2:294: recipe for target 'hostlib/hostLib/rjct/CMakeFiles/jrcpv1_server.dir/all' failed&lt;BR /&gt;| make[1]: *** [hostlib/hostLib/rjct/CMakeFiles/jrcpv1_server.dir/all] Error 2&lt;BR /&gt;| make[1]: *** Waiting for unfinished jobs....&lt;BR /&gt;| Scanning dependencies of target SSS_APIs&lt;BR /&gt;| [ 26%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/fsl_sss_apis.c.o&lt;BR /&gt;| [ 27%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/fsl_sss_util_asn1_der.c.o&lt;BR /&gt;| [ 28%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/fsl_sss_util_rsa_sign_utils.c.o&lt;BR /&gt;| [ 29%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/sscp/fsl_sss_sscp.c.o&lt;BR /&gt;| [ 30%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/a71cl/fsl_sscp_a71cl.c.o&lt;BR /&gt;| [ 31%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/a71ch/fsl_sscp_a71ch.c.o&lt;BR /&gt;| [ 31%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/se05x/fsl_sss_se05x_apis.c.o&lt;BR /&gt;| [ 32%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/se05x/fsl_sss_se05x_fastscp.c.o&lt;BR /&gt;| [ 33%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/se05x/fsl_sss_se05x_mw.c.o&lt;BR /&gt;| [ 34%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/se05x/fsl_sss_se05x_policy.c.o&lt;BR /&gt;| [ 35%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/se05x/fsl_sss_se05x_scp03.c.o&lt;BR /&gt;| [ 36%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/mbedtls/fsl_sss_mbedtls_apis.c.o&lt;BR /&gt;| [ 36%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/openssl/fsl_sss_openssl_apis.c.o&lt;BR /&gt;| [ 37%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/keystore/keystore_cmn.c.o&lt;BR /&gt;| [ 38%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/keystore/keystore_openssl.c.o&lt;BR /&gt;| [ 39%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/keystore/keystore_pc.c.o&lt;BR /&gt;| [ 40%] Building C object sss/CMakeFiles/SSS_APIs.dir/src/a71cx_common/fsl_sss_a71cx_cmn.c.o&lt;BR /&gt;| [ 41%] Linking C static library libSSS_APIs.a&lt;BR /&gt;| [ 41%] Built target SSS_APIs&lt;BR /&gt;| Makefile:129: recipe for target 'all' failed&lt;BR /&gt;| make: *** [all] Error 2&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/antonio/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/se050x/1.0-r0/temp/log.do_compile.28660)&lt;BR /&gt;ERROR: Task (/home/antonio/var-fsl-yocto/sources/meta-webserver/recipes-se050x/se050x/se050x.bb:do_compile) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 788 tasks of which 787 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt;&amp;nbsp; /home/antonio/var-fsl-yocto/sources/meta-webserver/recipes-se050x/se050x/se050x.bb:do_compile&lt;BR /&gt;Summary: There were 8 WARNING messages shown.&lt;BR /&gt;Summary: There were 2 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 11:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/975251#M122</guid>
      <dc:creator>antonio_mendes</dc:creator>
      <dc:date>2020-03-03T11:49:10Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto recipe for SE050x</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/975252#M123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured it out. I will leave the recipe here. Just put the ZIP inside.&lt;/P&gt;&lt;P&gt;I add success using imx8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DO NOT FORGET TO CHANGE I2C PORT (patch in recipe do this for me)!&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2020 12:14:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/975252#M123</guid>
      <dc:creator>antonio_mendes</dc:creator>
      <dc:date>2020-03-04T12:14:05Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto recipe for SE050x</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/975253#M124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the sharing!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2020 05:10:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/975253#M124</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-03-05T05:10:21Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto recipe for SE050x</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/1258091#M481</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We develop an updated .bb recipe for Yocto Zeus. Attached to this thread.&lt;/P&gt;&lt;P&gt;Thanks to&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/104654"&gt;@ettorechimenti&lt;/a&gt;&amp;nbsp;&amp;nbsp;and&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/145740"&gt;@tommaso_merciai&lt;/a&gt; from SECO&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Apr 2021 14:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/1258091#M481</guid>
      <dc:creator>tommaso_merciai</dc:creator>
      <dc:date>2021-04-07T14:50:37Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto recipe for SE050x</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/1493951#M848</link>
      <description>&lt;P&gt;Btw there is a Yocto recipe inside EdgeLock SE05x Plug &amp;amp; Trust Middleware zip file under:&lt;/P&gt;&lt;PRE&gt;simw-top\scripts\yocto\&lt;/PRE&gt;</description>
      <pubDate>Fri, 22 Jul 2022 09:24:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Yocto-recipe-for-SE050x/m-p/1493951#M848</guid>
      <dc:creator>cicicok</dc:creator>
      <dc:date>2022-07-22T09:24:09Z</dc:date>
    </item>
  </channel>
</rss>