<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Platform SCP keys in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Platform-SCP-keys/m-p/1630730#M1224</link>
    <description>&lt;P&gt;Maybe I missed that in the documentation, but when the SCP keys are rotated using SCPInitializeUpdate as described in GlobalPlatform Technology Secure Channel Protocol '03' Card Specification v2.3 – Amendment D, do the the Platform SCP keys listed in AN12436 for the specific chip become invalid and it is no longer possible to establish SCP using those keys?&lt;/P&gt;</description>
    <pubDate>Mon, 10 Apr 2023 20:55:43 GMT</pubDate>
    <dc:creator>bboozzoo</dc:creator>
    <dc:date>2023-04-10T20:55:43Z</dc:date>
    <item>
      <title>Platform SCP keys</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Platform-SCP-keys/m-p/1630730#M1224</link>
      <description>&lt;P&gt;Maybe I missed that in the documentation, but when the SCP keys are rotated using SCPInitializeUpdate as described in GlobalPlatform Technology Secure Channel Protocol '03' Card Specification v2.3 – Amendment D, do the the Platform SCP keys listed in AN12436 for the specific chip become invalid and it is no longer possible to establish SCP using those keys?&lt;/P&gt;</description>
      <pubDate>Mon, 10 Apr 2023 20:55:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Platform-SCP-keys/m-p/1630730#M1224</guid>
      <dc:creator>bboozzoo</dc:creator>
      <dc:date>2023-04-10T20:55:43Z</dc:date>
    </item>
    <item>
      <title>Re: Platform SCP keys</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Platform-SCP-keys/m-p/1630796#M1226</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211159"&gt;@bboozzoo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, after rotation, t&lt;SPAN&gt;he Platform SCP03 keys used during initial authentication will be replaced&amp;nbsp;with the new keys, but if you save the old keys somewhere, it is also possible to rotate them back.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Apr 2023 01:24:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Platform-SCP-keys/m-p/1630796#M1226</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-04-11T01:24:56Z</dc:date>
    </item>
  </channel>
</rss>