<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Do not use ISO7816/14443 interface in SE050 in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965405#M121</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Sep 2019 06:54:45 GMT</pubDate>
    <dc:creator>george</dc:creator>
    <dc:date>2019-09-27T06:54:45Z</dc:date>
    <item>
      <title>Do not use ISO7816/14443 interface in SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965401#M117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear NXP team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We will use SE050 for our new product.&lt;/P&gt;&lt;P&gt;However, our product does not use ISO7816 and ISO14443 Interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90317i495065FFE4BBA414/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ISO_14443_LA&lt;/P&gt;&lt;P&gt;ISO_14443_LB&lt;/P&gt;&lt;P&gt;ISO_7816_RST&lt;/P&gt;&lt;P&gt;ISO_7816_CLK&lt;/P&gt;&lt;P&gt;ISO_7816_IO&lt;/P&gt;&lt;P&gt;ISO_7816_IO2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How should these pins be terminated?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2019 13:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965401#M117</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2019-09-24T13:17:31Z</dc:date>
    </item>
    <item>
      <title>Re: Do not use ISO7816/14443 interface in SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965402#M118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello George,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not used, ISO7816 interface tied to VCC and ISO14443 interface tie to GND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 01:32:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965402#M118</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-09-25T01:32:05Z</dc:date>
    </item>
    <item>
      <title>Re: Do not use ISO7816/14443 interface in SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965403#M119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/Kan_Li"&gt;Kan_Li&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick reply.&lt;/P&gt;&lt;P&gt;Is my understanding correct below?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81549i1FDE98458B5CA9C8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And is the Pull Up/Down value about 10k-ohm appropriate?&lt;/P&gt;&lt;H3 data-reactid=".au9egkgx6o.1.0"&gt;&lt;/H3&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 09:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965403#M119</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2019-09-25T09:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: Do not use ISO7816/14443 interface in SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965404#M120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi George,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, that is ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Sep 2019 03:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965404#M120</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-09-27T03:13:21Z</dc:date>
    </item>
    <item>
      <title>Re: Do not use ISO7816/14443 interface in SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965405#M121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Sep 2019 06:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Do-not-use-ISO7816-14443-interface-in-SE050/m-p/965405#M121</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2019-09-27T06:54:45Z</dc:date>
    </item>
  </channel>
</rss>