<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックGet the ssscli tool to work without python</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Get-the-ssscli-tool-to-work-without-python/m-p/1601477#M1163</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to connect the Azure IoT Hub to my Android system which includes NXP Se050E over I2C.&lt;/P&gt;&lt;P&gt;I already succeeded to run the demo with&amp;nbsp;ex_sss_ecc.c file and sign using the NXP HSM.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Now I want to do the IoT HUB part.&lt;/P&gt;&lt;P&gt;According to&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12402.pdf" target="_self"&gt;your great tutorial&lt;/A&gt;, I need to create the certificate by the following commands:&lt;BR /&gt;a. Send &amp;gt; ssscli connect se050 t1oi2c 0.&lt;BR /&gt;b. Send &amp;gt; ssscli get cert 0xF0000101 ./device_cert.cer.&lt;BR /&gt;c. Send &amp;gt; ssscli refpem ecc pair 0xF0000100 ./reference_key.pem.&lt;BR /&gt;d. Send &amp;gt; ssscli disconnect.&lt;/P&gt;&lt;P&gt;Since I saw all the examples of the ssscli using python scripts, I didn't find a good way to run it on Android environment.&lt;BR /&gt;Is there an alternative ssscli tool, dedicated to c++ code?&lt;BR /&gt;If not, is there an example of how can I generate the certificate and the key by the c++ sss api?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Sun, 19 Feb 2023 18:38:46 GMT</pubDate>
    <dc:creator>nehadad</dc:creator>
    <dc:date>2023-02-19T18:38:46Z</dc:date>
    <item>
      <title>Get the ssscli tool to work without python</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Get-the-ssscli-tool-to-work-without-python/m-p/1601477#M1163</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to connect the Azure IoT Hub to my Android system which includes NXP Se050E over I2C.&lt;/P&gt;&lt;P&gt;I already succeeded to run the demo with&amp;nbsp;ex_sss_ecc.c file and sign using the NXP HSM.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Now I want to do the IoT HUB part.&lt;/P&gt;&lt;P&gt;According to&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12402.pdf" target="_self"&gt;your great tutorial&lt;/A&gt;, I need to create the certificate by the following commands:&lt;BR /&gt;a. Send &amp;gt; ssscli connect se050 t1oi2c 0.&lt;BR /&gt;b. Send &amp;gt; ssscli get cert 0xF0000101 ./device_cert.cer.&lt;BR /&gt;c. Send &amp;gt; ssscli refpem ecc pair 0xF0000100 ./reference_key.pem.&lt;BR /&gt;d. Send &amp;gt; ssscli disconnect.&lt;/P&gt;&lt;P&gt;Since I saw all the examples of the ssscli using python scripts, I didn't find a good way to run it on Android environment.&lt;BR /&gt;Is there an alternative ssscli tool, dedicated to c++ code?&lt;BR /&gt;If not, is there an example of how can I generate the certificate and the key by the c++ sss api?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Sun, 19 Feb 2023 18:38:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Get-the-ssscli-tool-to-work-without-python/m-p/1601477#M1163</guid>
      <dc:creator>nehadad</dc:creator>
      <dc:date>2023-02-19T18:38:46Z</dc:date>
    </item>
    <item>
      <title>Re: Get the ssscli tool to work without python</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Get-the-ssscli-tool-to-work-without-python/m-p/1601551#M1164</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212313"&gt;@nehadad&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, we provide another demo to fetch the cert in "simw-top\demos\se05x\se05x_GetCertificate", as well as a tool to create ref key file in "simw-top\demos\se05x\seTool", you may refer to "simw-top/doc/demos/se05x/seTool/Readme.html" for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 02:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Get-the-ssscli-tool-to-work-without-python/m-p/1601551#M1164</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-02-20T02:18:33Z</dc:date>
    </item>
    <item>
      <title>Re: Get the ssscli tool to work without python</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Get-the-ssscli-tool-to-work-without-python/m-p/1602151#M1167</link>
      <description>Thanks a lot!&lt;BR /&gt;I'll try it</description>
      <pubDate>Mon, 20 Feb 2023 16:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Get-the-ssscli-tool-to-work-without-python/m-p/1602151#M1167</guid>
      <dc:creator>nehadad</dc:creator>
      <dc:date>2023-02-20T16:37:45Z</dc:date>
    </item>
  </channel>
</rss>