<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: SE050: ISO14443 Can support also the B type ?</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-ISO14443-Can-support-also-the-B-type/m-p/960110#M116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, your understanding is correct. &lt;SPAN style="font-size: 11.0pt;"&gt;NXP cards so far always support only Type A.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Have a great day,&lt;BR /&gt;Kan &lt;BR /&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Sep 2019 05:46:47 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2019-09-11T05:46:47Z</dc:date>
    <item>
      <title>SE050: ISO14443 Can support also the B type ?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-ISO14443-Can-support-also-the-B-type/m-p/960109#M115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all, I see that the SE050Cx supports the ISO14443 RFID HF standard, but in the d.s. and other documentation is not clear if it supports also the ISO14443B standard, I see that it supports the Mifare that is an ISO14443A family.&lt;/P&gt;&lt;P&gt;Please clarify in the d.s.&lt;/P&gt;&lt;P&gt;I suppose it supports only the A type.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Sep 2019 10:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-ISO14443-Can-support-also-the-B-type/m-p/960109#M115</guid>
      <dc:creator>cant</dc:creator>
      <dc:date>2019-09-07T10:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: SE050: ISO14443 Can support also the B type ?</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-ISO14443-Can-support-also-the-B-type/m-p/960110#M116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, your understanding is correct. &lt;SPAN style="font-size: 11.0pt;"&gt;NXP cards so far always support only Type A.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Have a great day,&lt;BR /&gt;Kan &lt;BR /&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2019 05:46:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-ISO14443-Can-support-also-the-B-type/m-p/960110#M116</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-09-11T05:46:47Z</dc:date>
    </item>
  </channel>
</rss>