<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SAM AV3 generating ATR after PKI_ImportEccCurve command in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SAM-AV3-generating-ATR-after-PKI-ImportEccCurve-command/m-p/1589114#M1142</link>
    <description>&lt;P&gt;We have been using the SAM chips for many years now for MiFare support.&amp;nbsp; We have recently started investigating the ECC capabilities of the AV3 and have run into a peculiar problem.&amp;nbsp; Before we spend an extensive amount of time trying to figure out the root cause of the problem, I wanted to see if anyone had an explanation for what we are seeing.&lt;/P&gt;&lt;P&gt;When we issue the PKI_ImportEccCurve command, the SAM AV3 responds with a WTX request (0xC3).&amp;nbsp; Approximately 60ms after we respond with a WTX response block (0xE3), the AV3 appears to reboot because an ATR is sent out on the line again.&amp;nbsp; If we repeat the test without responding to the WTX request, the AV3 does not send out the ATR, but stalls (I'm assuming it's waiting for the WTX response, which is the behavior I would expect).&amp;nbsp; PKI_ImportEccKey, PKI_ExportEccPublicKey, and PKI_VerifyEccSignature all behave as expected at this point.&lt;/P&gt;&lt;P&gt;Anyone have any thoughts on this?&amp;nbsp; Have you seen it before?&amp;nbsp; Is the AV3 microcode broken?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 27 Jan 2023 22:56:09 GMT</pubDate>
    <dc:creator>Steven_Algn</dc:creator>
    <dc:date>2023-01-27T22:56:09Z</dc:date>
    <item>
      <title>SAM AV3 generating ATR after PKI_ImportEccCurve command</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SAM-AV3-generating-ATR-after-PKI-ImportEccCurve-command/m-p/1589114#M1142</link>
      <description>&lt;P&gt;We have been using the SAM chips for many years now for MiFare support.&amp;nbsp; We have recently started investigating the ECC capabilities of the AV3 and have run into a peculiar problem.&amp;nbsp; Before we spend an extensive amount of time trying to figure out the root cause of the problem, I wanted to see if anyone had an explanation for what we are seeing.&lt;/P&gt;&lt;P&gt;When we issue the PKI_ImportEccCurve command, the SAM AV3 responds with a WTX request (0xC3).&amp;nbsp; Approximately 60ms after we respond with a WTX response block (0xE3), the AV3 appears to reboot because an ATR is sent out on the line again.&amp;nbsp; If we repeat the test without responding to the WTX request, the AV3 does not send out the ATR, but stalls (I'm assuming it's waiting for the WTX response, which is the behavior I would expect).&amp;nbsp; PKI_ImportEccKey, PKI_ExportEccPublicKey, and PKI_VerifyEccSignature all behave as expected at this point.&lt;/P&gt;&lt;P&gt;Anyone have any thoughts on this?&amp;nbsp; Have you seen it before?&amp;nbsp; Is the AV3 microcode broken?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jan 2023 22:56:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SAM-AV3-generating-ATR-after-PKI-ImportEccCurve-command/m-p/1589114#M1142</guid>
      <dc:creator>Steven_Algn</dc:creator>
      <dc:date>2023-01-27T22:56:09Z</dc:date>
    </item>
    <item>
      <title>Re: SAM AV3 generating ATR after PKI_ImportEccCurve command</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SAM-AV3-generating-ATR-after-PKI-ImportEccCurve-command/m-p/1589296#M1143</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/187552"&gt;@Steven_Algn&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Details regarding&amp;nbsp; PKI_ImportEccCurve command are part of the document which is under NDA protect, so we are not allowed to discuss such topic in the public community. Is it possible to create a private ticket for this issue according to the following video?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/video/tutorial-for-nxp-support-case-portal:NCP-VIDEO" target="_blank"&gt;https://www.nxp.com/video/tutorial-for-nxp-support-case-portal:NCP-VIDEO&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please kindly attach the full log in the ticket for further analyzing.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your patience!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Sun, 29 Jan 2023 08:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SAM-AV3-generating-ATR-after-PKI-ImportEccCurve-command/m-p/1589296#M1143</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-01-29T08:45:41Z</dc:date>
    </item>
  </channel>
</rss>