<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Impossible to instantiate an encrypted communication between SE050 and IMXRT1170 in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Impossible-to-instantiate-an-encrypted-communication-between/m-p/1588789#M1141</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;please check the documentation &lt;A href="https://www.nxp.com/docs/en/application-note/AN12450.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12450.pdf&lt;/A&gt;&amp;nbsp;(EdgeLock SE05x Quick start guide with i.MX RT1060 and i.MX RT1170). In Section "6 Binding EdgeLock SE05x to a host using Platform SCP" the defines to be changed are shown to enable the encrypted channel for the demos and configure which keys are to be configured for the secure element demo board you have.&lt;/P&gt;
&lt;P&gt;Kind regards,&lt;BR /&gt;Michael&lt;/P&gt;</description>
    <pubDate>Fri, 27 Jan 2023 10:31:04 GMT</pubDate>
    <dc:creator>michaelsalfer</dc:creator>
    <dc:date>2023-01-27T10:31:04Z</dc:date>
    <item>
      <title>Impossible to instantiate an encrypted communication between SE050 and IMXRT1170</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Impossible-to-instantiate-an-encrypted-communication-between/m-p/1582427#M1138</link>
      <description>&lt;P&gt;I am experiencing a problem with the project "se05x_getInfo" included in SDK for IMXRT1170 ( SDK_2_12_1_MIMRT1170-EVK.zip).&lt;BR /&gt;I was unable to instantiate an encrypted communication between SE050 and IMXRT1170.&lt;BR /&gt;I made several attempts by modifying some #define but in vain.&lt;BR /&gt;What changes are needed to do this?&lt;/P&gt;&lt;P&gt;--------------------------------------------------------------&lt;BR /&gt;Further information&lt;BR /&gt;The demo ends correctly but with an unencrypted connection.&lt;BR /&gt;Log&lt;BR /&gt;App :INFO :PlugAndTrust_v04.01.01_20220112&lt;BR /&gt;sss :INFO :atr (Len=35)&lt;BR /&gt;00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08&lt;BR /&gt;01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41&lt;BR /&gt;54 50 4F&lt;BR /&gt;App :WARN :No SemsLite Applet Available.&lt;BR /&gt;sss :INFO :atr (Len=35)&lt;BR /&gt;00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08&lt;BR /&gt;01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41&lt;BR /&gt;54 50 4F&lt;BR /&gt;sss :WARN :Communication channel is Plain.&lt;BR /&gt;sss :WARN :!!!Not recommended for production use.!!!&lt;BR /&gt;App :WARN :#####################################################&lt;BR /&gt;App :INFO :uid (Len=18)&lt;BR /&gt;04 00 50 01 DB E9 7D 68 11 87 D8 04 7F 8B DA 0F&lt;BR /&gt;68 80&lt;BR /&gt;App :WARN :#####################################################&lt;BR /&gt;App :INFO :Applet Major = 3&lt;BR /&gt;App :INFO :Applet Minor = 1&lt;BR /&gt;App :INFO :Applet patch = 0&lt;BR /&gt;App :INFO :AppletConfig = 6FFF&lt;BR /&gt;App :INFO :With ECDAA&lt;BR /&gt;App :INFO :With ECDSA_ECDH_ECDHE&lt;BR /&gt;App :INFO :With EDDSA&lt;BR /&gt;App :INFO :With DH_MONT&lt;BR /&gt;App :INFO :With HMAC&lt;BR /&gt;App :INFO :With RSA_PLAIN&lt;BR /&gt;App :INFO :With RSA_CRT&lt;BR /&gt;App :INFO :With AES&lt;BR /&gt;App :INFO :With DES&lt;BR /&gt;App :INFO :With PBKDF&lt;BR /&gt;App :INFO :With TLS&lt;BR /&gt;App :INFO :With MIFARE&lt;BR /&gt;App :INFO :With I2CM&lt;BR /&gt;App :INFO :Internal = 010B&lt;BR /&gt;App :WARN :#####################################################&lt;BR /&gt;App :INFO :Tag value - proprietary data 0xFE = 0xFE&lt;BR /&gt;App :INFO :Length of following data 0x45 = 0x45&lt;BR /&gt;App :INFO :Tag card identification data (Len=2)&lt;BR /&gt;DF 28&lt;BR /&gt;App :INFO :Length of card identification data = 0x42&lt;BR /&gt;App :INFO :Tag configuration ID (Must be 0x01) = 0x01&lt;BR /&gt;App :INFO :Configuration ID (Len=12)&lt;BR /&gt;00 04 A1 F4 45 88 4F 17 E5 19 C0 69&lt;BR /&gt;App :INFO :OEF ID (Len=2)&lt;BR /&gt;A1 F4&lt;BR /&gt;App :INFO :Tag patch ID (Must be 0x02) = 0x02&lt;BR /&gt;App :INFO :Patch ID (Len=8)&lt;BR /&gt;00 00 00 00 00 00 00 01&lt;BR /&gt;App :INFO :Tag platform build ID1 (Must be 0x03) = 0x03&lt;BR /&gt;App :INFO :Platform build ID (Len=24)&lt;BR /&gt;4A 33 52 33 35 31 30 32 31 45 45 45 30 34 30 30&lt;BR /&gt;BC 03 04 79 33 8D 18 10&lt;BR /&gt;App :INFO :JCOP Platform ID = J3R351021EEE0400&lt;BR /&gt;App :INFO :Tag FIPS mode (Must be 0x05) = 0x05&lt;BR /&gt;App :INFO :FIPS mode var = 0x00&lt;BR /&gt;App :INFO :Tag pre-perso state (Must be 0x07) = 0x07&lt;BR /&gt;App :INFO :Bit mask of pre-perso state var = 0x00&lt;BR /&gt;App :INFO :Tag ROM ID (Must be 0x08) = 0x08&lt;BR /&gt;App :INFO :ROM ID (Len=8)&lt;BR /&gt;2E 5A D8 84 09 C9 BA DB&lt;BR /&gt;App :INFO :Status Word (SW) (Len=2)&lt;BR /&gt;90 00&lt;BR /&gt;App :INFO :se05x_GetInfoPlainApplet Example Success !!!...&lt;BR /&gt;App :WARN :#####################################################&lt;BR /&gt;App :INFO :cplc_data.IC_fabricator (Len=2)&lt;BR /&gt;47 90&lt;BR /&gt;App :INFO :cplc_data.IC_type1 (Len=2)&lt;BR /&gt;D3 21&lt;BR /&gt;App :INFO :cplc_data.Operating_system_identifier (Len=2)&lt;BR /&gt;47 00&lt;BR /&gt;App :INFO :cplc_data.Operating_system_release_date (Len=2)&lt;BR /&gt;00 00&lt;BR /&gt;App :INFO :cplc_data.Operating_system_release_level (Len=2)&lt;BR /&gt;00 00&lt;BR /&gt;App :INFO :cplc_data.IC_fabrication_date (Len=2)&lt;BR /&gt;92 84&lt;BR /&gt;App :INFO :cplc_data.IC_Serial_number (Len=4)&lt;BR /&gt;06 06 88 99&lt;BR /&gt;App :INFO :cplc_data.IC_Batch_identifier (Len=2)&lt;BR /&gt;37 34&lt;BR /&gt;App :INFO :cplc_data.IC_module_fabricator (Len=2)&lt;BR /&gt;00 00&lt;BR /&gt;App :INFO :cplc_data.IC_module_packaging_date (Len=2)&lt;BR /&gt;00 00&lt;BR /&gt;App :INFO :cplc_data.ICC_manufacturer (Len=2)&lt;BR /&gt;00 00&lt;BR /&gt;App :INFO :cplc_data.IC_embedding_date (Len=2)&lt;BR /&gt;00 00&lt;BR /&gt;App :INFO :cplc_data.IC_OS_initializer (Len=2)&lt;BR /&gt;03 7F&lt;BR /&gt;App :INFO :cplc_data.IC_OS_initialization_date (Len=2)&lt;BR /&gt;8B 36&lt;BR /&gt;App :INFO :cplc_data.IC_OS_initialization_equipment (Len=4)&lt;BR /&gt;30 36 38 38&lt;BR /&gt;App :INFO :cplc_data.IC_personalizer (Len=2)&lt;BR /&gt;00 00&lt;BR /&gt;App :INFO :cplc_data.IC_personalization_date (Len=2)&lt;BR /&gt;00 00&lt;BR /&gt;App :INFO :cplc_data.IC_personalization_equipment_ID (Len=4)&lt;BR /&gt;00 00 00 00&lt;BR /&gt;App :INFO :cplc_data.SW (Len=2)&lt;BR /&gt;90 00&lt;BR /&gt;App :INFO :ex_sss Finished&lt;/P&gt;</description>
      <pubDate>Fri, 13 Jan 2023 11:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Impossible-to-instantiate-an-encrypted-communication-between/m-p/1582427#M1138</guid>
      <dc:creator>stefanotatini</dc:creator>
      <dc:date>2023-01-13T11:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: Impossible to instantiate an encrypted communication between SE050 and IMXRT1170</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Impossible-to-instantiate-an-encrypted-communication-between/m-p/1588789#M1141</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;please check the documentation &lt;A href="https://www.nxp.com/docs/en/application-note/AN12450.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12450.pdf&lt;/A&gt;&amp;nbsp;(EdgeLock SE05x Quick start guide with i.MX RT1060 and i.MX RT1170). In Section "6 Binding EdgeLock SE05x to a host using Platform SCP" the defines to be changed are shown to enable the encrypted channel for the demos and configure which keys are to be configured for the secure element demo board you have.&lt;/P&gt;
&lt;P&gt;Kind regards,&lt;BR /&gt;Michael&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jan 2023 10:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Impossible-to-instantiate-an-encrypted-communication-between/m-p/1588789#M1141</guid>
      <dc:creator>michaelsalfer</dc:creator>
      <dc:date>2023-01-27T10:31:04Z</dc:date>
    </item>
  </channel>
</rss>