<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: A70CM Update to OpenSSL 1.1</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957536#M111</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I know, A70CM is an old SE product, now we recommend SE050 for new design, and the hostlib for SE050 has support for OpenSSL 1.1. Please kindly refer to &lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=se050_mw_v02.10.00" title="https://www.nxp.com/webapp/Download?colCode=se050_mw_v02.10.00"&gt;https://www.nxp.com/webapp/Download?colCode=se050_mw_v02.10.00&lt;/A&gt;&amp;nbsp; for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jul 2019 05:39:24 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2019-07-26T05:39:24Z</dc:date>
    <item>
      <title>A70CM Update to OpenSSL 1.1</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957535#M110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We currently have a product with an A70CM Secure Element that connects to a cloud. It is currently using OpenSSL 1.0. Due to security concerns we need to update to OpenSSL 1.1. Is there an update to the hostlib library ? If so how do I obtain it ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 18:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957535#M110</guid>
      <dc:creator>william_duroche</dc:creator>
      <dc:date>2019-07-23T18:33:32Z</dc:date>
    </item>
    <item>
      <title>Re: A70CM Update to OpenSSL 1.1</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957536#M111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I know, A70CM is an old SE product, now we recommend SE050 for new design, and the hostlib for SE050 has support for OpenSSL 1.1. Please kindly refer to &lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=se050_mw_v02.10.00" title="https://www.nxp.com/webapp/Download?colCode=se050_mw_v02.10.00"&gt;https://www.nxp.com/webapp/Download?colCode=se050_mw_v02.10.00&lt;/A&gt;&amp;nbsp; for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2019 05:39:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957536#M111</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-07-26T05:39:24Z</dc:date>
    </item>
    <item>
      <title>Re: A70CM Update to OpenSSL 1.1</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957537#M112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the response. Looking through the code for the SE050 I do not see the corresponding A70 files. Are they replaced by the A71 files ? Which version is closest A71CH or A71CL ? Or should I look toward se05x ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2019 12:54:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957537#M112</guid>
      <dc:creator>william_duroche</dc:creator>
      <dc:date>2019-07-31T12:54:39Z</dc:date>
    </item>
    <item>
      <title>Re: A70CM Update to OpenSSL 1.1</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957538#M113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello William,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may the openssl lib in the folder of&amp;nbsp; "se050_mw_v02.10.00\simw-top\ext\openssl".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2019 02:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957538#M113</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-08-01T02:12:02Z</dc:date>
    </item>
    <item>
      <title>Re: A70CM Update to OpenSSL 1.1</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957539#M114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank your for the answer. I will look into this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2019 13:30:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A70CM-Update-to-OpenSSL-1-1/m-p/957539#M114</guid>
      <dc:creator>william_duroche</dc:creator>
      <dc:date>2019-08-01T13:30:14Z</dc:date>
    </item>
  </channel>
</rss>