<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックIntegrate ES 8266 Project with A71ch</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Integrate-ES-8266-Project-with-A71ch/m-p/811591#M11</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am trying to integrate two standalone projects&lt;/P&gt;&lt;P&gt;1. Connecting &lt;STRONG&gt;FRDM k64 F&lt;/STRONG&gt; board to WiFi through&lt;STRONG&gt; ESP8266&lt;/STRONG&gt; module(Using&amp;nbsp;&lt;STRONG&gt;MCU&amp;nbsp;xpresso&lt;/STRONG&gt; - I converted the code from &lt;STRONG&gt;Mbed&lt;/STRONG&gt; for this)&lt;/P&gt;&lt;P&gt;2. Standalone application of uploading the data from &lt;STRONG&gt;Frdm k64F to IBM Watson using A71ch.&lt;/STRONG&gt; (&lt;STRONG&gt;MCU xpresso&lt;/STRONG&gt;.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both the projects are working successfully when I compile them independently. But when I try to integrate them, I am facing issues in linking the files.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The mbed.h file in esp8266 project is interfering with other library files in A71ch demo.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The library files in A71ch demo are not getting successfully&amp;nbsp;imported&amp;nbsp;when I try to move it to esp 8266 project.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The goal of my project is connect the FRDM board with esp module and upload&amp;nbsp;the data to IBM using a71ch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if the project I am trying to do is possible in this way. Any pointers would be highly helpful. I have attached project file for esp 8266 and&lt;STRONG&gt;&amp;nbsp;link for&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12186.pdf" title="https://www.nxp.com/docs/en/application-note/AN12186.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12186.pdf&lt;/A&gt;&lt;/STRONG&gt;&amp;nbsp; for A71ch project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Niranjan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Nov 2018 05:58:36 GMT</pubDate>
    <dc:creator>trialaccount12</dc:creator>
    <dc:date>2018-11-07T05:58:36Z</dc:date>
    <item>
      <title>Integrate ES 8266 Project with A71ch</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Integrate-ES-8266-Project-with-A71ch/m-p/811591#M11</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am trying to integrate two standalone projects&lt;/P&gt;&lt;P&gt;1. Connecting &lt;STRONG&gt;FRDM k64 F&lt;/STRONG&gt; board to WiFi through&lt;STRONG&gt; ESP8266&lt;/STRONG&gt; module(Using&amp;nbsp;&lt;STRONG&gt;MCU&amp;nbsp;xpresso&lt;/STRONG&gt; - I converted the code from &lt;STRONG&gt;Mbed&lt;/STRONG&gt; for this)&lt;/P&gt;&lt;P&gt;2. Standalone application of uploading the data from &lt;STRONG&gt;Frdm k64F to IBM Watson using A71ch.&lt;/STRONG&gt; (&lt;STRONG&gt;MCU xpresso&lt;/STRONG&gt;.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both the projects are working successfully when I compile them independently. But when I try to integrate them, I am facing issues in linking the files.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The mbed.h file in esp8266 project is interfering with other library files in A71ch demo.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The library files in A71ch demo are not getting successfully&amp;nbsp;imported&amp;nbsp;when I try to move it to esp 8266 project.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The goal of my project is connect the FRDM board with esp module and upload&amp;nbsp;the data to IBM using a71ch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if the project I am trying to do is possible in this way. Any pointers would be highly helpful. I have attached project file for esp 8266 and&lt;STRONG&gt;&amp;nbsp;link for&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12186.pdf" title="https://www.nxp.com/docs/en/application-note/AN12186.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12186.pdf&lt;/A&gt;&lt;/STRONG&gt;&amp;nbsp; for A71ch project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Niranjan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2018 05:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Integrate-ES-8266-Project-with-A71ch/m-p/811591#M11</guid>
      <dc:creator>trialaccount12</dc:creator>
      <dc:date>2018-11-07T05:58:36Z</dc:date>
    </item>
    <item>
      <title>Re: Integrate ES 8266 Project with A71ch</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Integrate-ES-8266-Project-with-A71ch/m-p/811592#M12</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looks like it is a porting issue , and there is an app note on that topic, please refer to &lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12185.pdf" title="https://www.nxp.com/docs/en/application-note/AN12185.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12185.pdf&lt;/A&gt;&amp;nbsp; for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 06:39:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Integrate-ES-8266-Project-with-A71ch/m-p/811592#M12</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2018-11-21T06:39:55Z</dc:date>
    </item>
  </channel>
</rss>