<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: Hardware reset jumper on SE050ARD-E</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Hardware-reset-jumper-on-SE050ARD-E/m-p/1576323#M1088</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210414"&gt;@psvz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No, it doesn't erase any key in the SE050, this signal routes to the reset pin of ISO7816 interface, which is pin 14 of SE050. To connect OM-SE050ARD-E with a Raspberry Pi board, it would be much easier with a&amp;nbsp; OM-SE05xRPI board, or via wires as mentioned in&amp;nbsp;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12570.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12570.pdf&lt;/A&gt;&amp;nbsp;. Please kindly refer to "2.1.2.1 Using the OM-SE05xRPI adapter board" or "2.1.2.2 Connecting the OM-SE05xARD with wires" for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Tue, 03 Jan 2023 05:49:24 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2023-01-03T05:49:24Z</dc:date>
    <item>
      <title>Hardware reset jumper on SE050ARD-E</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Hardware-reset-jumper-on-SE050ARD-E/m-p/1575908#M1078</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Re&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13539.pdf" target="_blank"&gt;OM-SE05xARD hardware overview (nxp.com)&lt;/A&gt;&amp;nbsp;section 4.4&lt;/P&gt;&lt;P&gt;Could you please confirm what does "reset" mean? Does it erase any keys inside SE050?&amp;nbsp;&lt;/P&gt;&lt;P&gt;In configuration with Raspberry Pi - which pins I need to close on J12 to trigger reset - it is not clear from that document.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Sat, 31 Dec 2022 22:50:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Hardware-reset-jumper-on-SE050ARD-E/m-p/1575908#M1078</guid>
      <dc:creator>psvz</dc:creator>
      <dc:date>2022-12-31T22:50:06Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware reset jumper on SE050ARD-E</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Hardware-reset-jumper-on-SE050ARD-E/m-p/1576323#M1088</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210414"&gt;@psvz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No, it doesn't erase any key in the SE050, this signal routes to the reset pin of ISO7816 interface, which is pin 14 of SE050. To connect OM-SE050ARD-E with a Raspberry Pi board, it would be much easier with a&amp;nbsp; OM-SE05xRPI board, or via wires as mentioned in&amp;nbsp;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12570.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12570.pdf&lt;/A&gt;&amp;nbsp;. Please kindly refer to "2.1.2.1 Using the OM-SE05xRPI adapter board" or "2.1.2.2 Connecting the OM-SE05xARD with wires" for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jan 2023 05:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Hardware-reset-jumper-on-SE050ARD-E/m-p/1576323#M1088</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-01-03T05:49:24Z</dc:date>
    </item>
  </channel>
</rss>