<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic API for secure objects' origin in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/API-for-secure-objects-origin/m-p/1575218#M1068</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;Could you please confirm how could I read or change the ORIGIN of a secure object (key) - I cannot find such API. I would like to read and/or inject this property with my keys:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;enum SE05x_Origin_t
Where was this object originated

Values:

kSE05x_Origin_NA = 0
Invalid

kSE05x_Origin_EXTERNAL = 0x01
Generated outside the module.

kSE05x_Origin_INTERNAL = 0x02
Generated inside the module.

kSE05x_Origin_PROVISIONED = 0x03
Trust provisioned by NXP&lt;/LI-CODE&gt;</description>
    <pubDate>Wed, 28 Dec 2022 13:50:59 GMT</pubDate>
    <dc:creator>psvz</dc:creator>
    <dc:date>2022-12-28T13:50:59Z</dc:date>
    <item>
      <title>API for secure objects' origin</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/API-for-secure-objects-origin/m-p/1575218#M1068</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;Could you please confirm how could I read or change the ORIGIN of a secure object (key) - I cannot find such API. I would like to read and/or inject this property with my keys:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;enum SE05x_Origin_t
Where was this object originated

Values:

kSE05x_Origin_NA = 0
Invalid

kSE05x_Origin_EXTERNAL = 0x01
Generated outside the module.

kSE05x_Origin_INTERNAL = 0x02
Generated inside the module.

kSE05x_Origin_PROVISIONED = 0x03
Trust provisioned by NXP&lt;/LI-CODE&gt;</description>
      <pubDate>Wed, 28 Dec 2022 13:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/API-for-secure-objects-origin/m-p/1575218#M1068</guid>
      <dc:creator>psvz</dc:creator>
      <dc:date>2022-12-28T13:50:59Z</dc:date>
    </item>
    <item>
      <title>Re: API for secure objects' origin</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/API-for-secure-objects-origin/m-p/1575339#M1071</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210414"&gt;@psvz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am sorry, but there is no API to inject&amp;nbsp;&lt;SPAN&gt;this property, you may just read this with the help of readobject command, indeed it is one of the object&amp;nbsp;attributes that is updated during applet runtime for Secure Objects of type AESKey, DESKey, HMACKey, ECKey and&lt;BR /&gt;RSAKey only and does not get updated for other object types.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12413.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12413.pdf&lt;/A&gt;&amp;nbsp;for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 29 Dec 2022 01:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/API-for-secure-objects-origin/m-p/1575339#M1071</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-12-29T01:51:34Z</dc:date>
    </item>
  </channel>
</rss>