<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure Authentication中的主题 Re: Generate RSA fails, ssscli</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Generate-RSA-fails-ssscli/m-p/1574904#M1057</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;is it only for "generate" that isn't supported - can I inject my own RSA 4096 bits key? Besides, is there any EC-type key that SE050 can use to decrypt a message e.g., 25519 curve can be used for encrypt/decrypt (check&amp;nbsp;&lt;A href="https://pynacl.readthedocs.io/en/latest/secret/" target="_blank"&gt;Secret Key Encryption — PyNaCl 1.6.0.dev1 documentation&lt;/A&gt;) but you could use other EC keys for that...&lt;/P&gt;</description>
    <pubDate>Tue, 27 Dec 2022 11:24:18 GMT</pubDate>
    <dc:creator>psvz</dc:creator>
    <dc:date>2022-12-27T11:24:18Z</dc:date>
    <item>
      <title>Generate RSA fails, ssscli</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Generate-RSA-fails-ssscli/m-p/1574610#M1046</link>
      <description>&lt;P&gt;SE050-E&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@raspberrypi:~ # ssscli generate rsa abc 4096
Generating RSA Key Pair at KeyID = 0x00000ABC,  bits=4096
sss   :INFO :atr (Len=35)
      01 A0 00 00    03 96 04 03    E8 00 FE 02    0B 03 E8 00
      01 00 00 00    00 64 13 88    0A 00 65 53    45 30 35 31
      00 00 00
ERROR:sss.keystore:sss_key_store_generate_key FAILED
ERROR! Could not generate RSA Key Pair at KeyID 0x00000ABC&lt;/LI-CODE&gt;&lt;P&gt;any idea?&lt;/P&gt;</description>
      <pubDate>Mon, 26 Dec 2022 11:36:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Generate-RSA-fails-ssscli/m-p/1574610#M1046</guid>
      <dc:creator>psvz</dc:creator>
      <dc:date>2022-12-26T11:36:20Z</dc:date>
    </item>
    <item>
      <title>Re: Generate RSA fails, ssscli</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Generate-RSA-fails-ssscli/m-p/1574759#M1055</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210414"&gt;@psvz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;RSA is not supported on SE050-E, please use SE051/SE050F instead for that purpose.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the confusion that has caused.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 27 Dec 2022 03:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Generate-RSA-fails-ssscli/m-p/1574759#M1055</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-12-27T03:31:05Z</dc:date>
    </item>
    <item>
      <title>Re: Generate RSA fails, ssscli</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Generate-RSA-fails-ssscli/m-p/1574904#M1057</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;is it only for "generate" that isn't supported - can I inject my own RSA 4096 bits key? Besides, is there any EC-type key that SE050 can use to decrypt a message e.g., 25519 curve can be used for encrypt/decrypt (check&amp;nbsp;&lt;A href="https://pynacl.readthedocs.io/en/latest/secret/" target="_blank"&gt;Secret Key Encryption — PyNaCl 1.6.0.dev1 documentation&lt;/A&gt;) but you could use other EC keys for that...&lt;/P&gt;</description>
      <pubDate>Tue, 27 Dec 2022 11:24:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Generate-RSA-fails-ssscli/m-p/1574904#M1057</guid>
      <dc:creator>psvz</dc:creator>
      <dc:date>2022-12-27T11:24:18Z</dc:date>
    </item>
    <item>
      <title>Re: Generate RSA fails, ssscli</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Generate-RSA-fails-ssscli/m-p/1575038#M1063</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210414"&gt;@psvz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No, I mean the RSA&amp;nbsp;algorithms are not supported on SE050-E. You may generate an ECC Key pair instead for&amp;nbsp;&lt;SPAN&gt;encrypt/decrypt purpose.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1672195900379.png" style="width: 542px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205568i8A7D87EAFFEC77D4/image-dimensions/542x317?v=v2" width="542" height="317" role="button" title="Kan_Li_0-1672195900379.png" alt="Kan_Li_0-1672195900379.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Dec 2022 02:52:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Generate-RSA-fails-ssscli/m-p/1575038#M1063</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-12-28T02:52:09Z</dc:date>
    </item>
  </channel>
</rss>