<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックSE050: Mifare SAM functionality + current consumption</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Mifare-SAM-functionality-current-consumption/m-p/946309#M103</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have several questions about the SE050.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- The data sheet says that the SE050 also has a "MIFARE SAM functionality". But I didn't find any further information about it, neither in the datasheet nor in the application notes. When will more information on this topic be available?&lt;/P&gt;&lt;P&gt;- In the data sheet under "14.1.3 Power consumption" the currents of the SE050 in the different operating modes are indicated. How high is the supply voltage for this information?&lt;/P&gt;&lt;P&gt;- In the data sheet it is stated under "14.1.3 Power consumption" that fCPU=48MHz. Is it possible to operate the SE050 with a slower clock frequency to further reduce the current?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jun 2019 10:40:44 GMT</pubDate>
    <dc:creator>timriddermann</dc:creator>
    <dc:date>2019-06-19T10:40:44Z</dc:date>
    <item>
      <title>SE050: Mifare SAM functionality + current consumption</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Mifare-SAM-functionality-current-consumption/m-p/946309#M103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have several questions about the SE050.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- The data sheet says that the SE050 also has a "MIFARE SAM functionality". But I didn't find any further information about it, neither in the datasheet nor in the application notes. When will more information on this topic be available?&lt;/P&gt;&lt;P&gt;- In the data sheet under "14.1.3 Power consumption" the currents of the SE050 in the different operating modes are indicated. How high is the supply voltage for this information?&lt;/P&gt;&lt;P&gt;- In the data sheet it is stated under "14.1.3 Power consumption" that fCPU=48MHz. Is it possible to operate the SE050 with a slower clock frequency to further reduce the current?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 10:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Mifare-SAM-functionality-current-consumption/m-p/946309#M103</guid>
      <dc:creator>timriddermann</dc:creator>
      <dc:date>2019-06-19T10:40:44Z</dc:date>
    </item>
    <item>
      <title>Re: SE050: Mifare SAM functionality + current consumption</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Mifare-SAM-functionality-current-consumption/m-p/946310#M104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- The data sheet says that the SE050 also has a "MIFARE SAM functionality". But I didn't find any further information about it, neither in the datasheet nor in the application notes. When will more information on this topic be available?&lt;/P&gt;&lt;P&gt;- There will be a demo on this topic soon, please follow this product as below to get the notification when it is available.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89665i9B621E0172A06E44/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- In the data sheet under "14.1.3 Power consumption" the currents of the SE050 in the different operating modes are indicated. How high is the supply voltage for this information?&lt;/P&gt;&lt;P&gt;-Please refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89666iD1FAE5D844BE3A7D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- In the data sheet it is stated under "14.1.3 Power consumption" that fCPU=48MHz. Is it possible to operate the SE050 with a slower clock frequency to further reduce the current?&lt;/P&gt;&lt;P&gt;-No, it is not possible, BTW, what is the usecase? &lt;SPAN style="font-size: 11.0pt;"&gt;why current consumption should be limited? Please help to clarify.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Have a great day,&lt;BR /&gt;Kan &lt;BR /&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jun 2019 03:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Mifare-SAM-functionality-current-consumption/m-p/946310#M104</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-06-25T03:15:32Z</dc:date>
    </item>
  </channel>
</rss>