<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: se05x_API_DeleteAll_Iterative() of Plug and trust middleware in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570880#M1025</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/150536"&gt;@kei_odagiri&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes,&amp;nbsp;&lt;SPAN&gt;the range of keyid from 1 to 0x7BFFFFFF is opened to users, but there are cases customers trust provision some secure objects there, and SE05X_OBJID_TP_MASK can be used to prevent deleting such kind of objects accidently , but of course users may adjust&amp;nbsp;SE05X_OBJID_TP_MASK definition according to their requirements.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope that makes sense,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 16 Dec 2022 02:12:52 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2022-12-16T02:12:52Z</dc:date>
    <item>
      <title>se05x_API_DeleteAll_Iterative() of Plug and trust middleware</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570187#M1022</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm developing an app to delete some secure objects of se050, so to speak a reset command. The app utilizes Se05x_API_DeleteAll_Iterative(), and I found a phenomenon that secure objects having keyid from 1 to 3 are not deleted. I did quick check for source code in plug and trust middle ware.&lt;/P&gt;&lt;P&gt;I think SE05X_OBJID_TP_MASK causes the &lt;SPAN&gt;phenomenon which the&amp;nbsp;&lt;/SPAN&gt;secure objects aren't deleted.&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/NXP/plug-and-trust/blob/v04.02.00/hostlib/hostLib/se05x/src/se05x_mw.c#L51" target="_blank" rel="noopener"&gt;https://github.com/NXP/plug-and-trust/blob/v04.02.00/hostlib/hostLib/se05x/src/se05x_mw.c#L51&lt;/A&gt;&lt;/P&gt;&lt;PRE&gt;            else if (!SE05X_OBJID_TP_MASK(id) &amp;amp;&amp;amp; id) {
                LOG_D("Not erasing Trust Provisioned objects");
            }&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/NXP/plug-and-trust/blob/v04.02.00/sss/ex/inc/ex_sss_objid.h#L31" target="_blank" rel="noopener"&gt;https://github.com/NXP/plug-and-trust/blob/v04.02.00/sss/ex/inc/ex_sss_objid.h#L31&lt;/A&gt;&lt;/P&gt;&lt;PRE&gt;#define SE05X_OBJID_TP_MASK(X)              (0xFFFFFFFC &amp;amp; (X))&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kei Odagiri&lt;/P&gt;&lt;P&gt;Atmark techno,Inc.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 06:18:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570187#M1022</guid>
      <dc:creator>kei_odagiri</dc:creator>
      <dc:date>2022-12-15T06:18:52Z</dc:date>
    </item>
    <item>
      <title>Re: se05x_API_DeleteAll_Iterative() of Plug and trust middleware</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570821#M1023</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Please let me add this information.&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to&amp;nbsp;AN13030 Plug &amp;amp; Trust MW Documentation (Rev. 1.9 — 30 June 2022), the range of keyid from 1 to 0x7BFFFFFF is opened to users. But users can't delete the keyid from 1 to 3 by using&amp;nbsp;&lt;SPAN&gt;Se05x_API_DeleteAll_Iterative().&amp;nbsp;&lt;/SPAN&gt;I think the implementation of the&amp;nbsp;&lt;SPAN&gt;Se05x_API_DeleteAll_Iterative() does not allow it.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;3.14 Key Id Range and Purpose&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="se050_keyid_range.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/204654i8F05F7E8F54B747C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="se050_keyid_range.png" alt="se050_keyid_range.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Dec 2022 00:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570821#M1023</guid>
      <dc:creator>kei_odagiri</dc:creator>
      <dc:date>2022-12-16T00:06:14Z</dc:date>
    </item>
    <item>
      <title>Re: se05x_API_DeleteAll_Iterative() of Plug and trust middleware</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570826#M1024</link>
      <description>&lt;P&gt;I tried deleting manually the keyid range, I succeeded to delete the keyid. Therefore users can't delete the range by&amp;nbsp;se05x_API_DeleteAll_Iterative() but users can delete it by&amp;nbsp;&lt;SPAN&gt;Se05x_API_DeleteSecureObject().&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# ssscli erase 1&lt;BR /&gt;ssse-flw: EmbSe_Init(): Entry&lt;BR /&gt;App :INFO :Using PortName='/dev/i2c-2:0x48' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-2:0x48)&lt;BR /&gt;sss :INFO :atr (Len=35)&lt;BR /&gt;00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08&lt;BR /&gt;01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41&lt;BR /&gt;54 50 4F&lt;BR /&gt;sss :WARN :Communication channel is Plain.&lt;BR /&gt;sss :WARN :!!!Not recommended for production use.!!!&lt;BR /&gt;ssse-flw: Version: 1.0.5&lt;BR /&gt;ssse-flw: EmbSe_Init(): Exit&lt;BR /&gt;ssse-flw: Control Command EMBSE_LOG_LEVEL; requested log level = 7&lt;BR /&gt;Erasing Key entry from KeyID = 0x00000001&lt;BR /&gt;sss :INFO :atr (Len=35)&lt;BR /&gt;00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08&lt;BR /&gt;01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41&lt;BR /&gt;54 50 4F&lt;BR /&gt;sss :WARN :Communication channel is Plain.&lt;BR /&gt;sss :WARN :!!!Not recommended for production use.!!!&lt;BR /&gt;Erased Key entry from KeyID = 0x00000001&lt;BR /&gt;ssse-flw: EmbSe_Finish(): Entry&lt;BR /&gt;ssse-flw: EmbSe_Finish(): Exit&lt;BR /&gt;ssse-flw: EmbSe_Destroy(): Entry&lt;/P&gt;</description>
      <pubDate>Fri, 16 Dec 2022 00:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570826#M1024</guid>
      <dc:creator>kei_odagiri</dc:creator>
      <dc:date>2022-12-16T00:36:07Z</dc:date>
    </item>
    <item>
      <title>Re: se05x_API_DeleteAll_Iterative() of Plug and trust middleware</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570880#M1025</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/150536"&gt;@kei_odagiri&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes,&amp;nbsp;&lt;SPAN&gt;the range of keyid from 1 to 0x7BFFFFFF is opened to users, but there are cases customers trust provision some secure objects there, and SE05X_OBJID_TP_MASK can be used to prevent deleting such kind of objects accidently , but of course users may adjust&amp;nbsp;SE05X_OBJID_TP_MASK definition according to their requirements.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope that makes sense,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Dec 2022 02:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570880#M1025</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-12-16T02:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: se05x_API_DeleteAll_Iterative() of Plug and trust middleware</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570965#M1026</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276" target="_self"&gt;&lt;SPAN class=""&gt;Kan_Li&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I suspected there is a policy to protect NXP's special trust provisioning objects. Additionally, I considered the middle ware should implement the restriction for all apis. But, sure, if middle ware restrict to delete the keyid in all apis, users may not handle under unexpected situation.&lt;/P&gt;&lt;P&gt;Anyway since you mentioned users can adjust the protection, I will modify the range of the macro to my suitable spec.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Kei Odagiri&lt;/P&gt;</description>
      <pubDate>Fri, 16 Dec 2022 04:45:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/se05x-API-DeleteAll-Iterative-of-Plug-and-trust-middleware/m-p/1570965#M1026</guid>
      <dc:creator>kei_odagiri</dc:creator>
      <dc:date>2022-12-16T04:45:25Z</dc:date>
    </item>
  </channel>
</rss>