<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic A5000 RFU pins - inconsistent guidance in datasheet in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/A5000-RFU-pins-inconsistent-guidance-in-datasheet/m-p/1555266#M1005</link>
    <description>&lt;P&gt;I am replacing the SE050 with A5000 on my schematic. The NXP documentation mentions the parts are pin-to-pin compatible.&lt;/P&gt;&lt;P&gt;However, the Pin Description table of the datasheets for the two parts differ when describing the RFU pins (originally used for ISO 7816 interface):&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;A5000 datasheet (Rev 1.2) recommends&lt;UL&gt;&lt;LI&gt;pin 3 and 13 to VCC&lt;/LI&gt;&lt;LI&gt;pin 14 to VSS&lt;/LI&gt;&lt;LI&gt;pin 16 to VIN&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;SE050 datasheet (Rev 3.7) recommends&lt;UL&gt;&lt;LI&gt;pin 3, 13, and 16 NC&lt;/LI&gt;&lt;LI&gt;pin 14 to VSS or VCC&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Which one is correct? Ideally I'd like to NC as many pins as possible to simplify layout routing.&lt;/P&gt;</description>
    <pubDate>Wed, 16 Nov 2022 21:26:35 GMT</pubDate>
    <dc:creator>michaelh2</dc:creator>
    <dc:date>2022-11-16T21:26:35Z</dc:date>
    <item>
      <title>A5000 RFU pins - inconsistent guidance in datasheet</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A5000-RFU-pins-inconsistent-guidance-in-datasheet/m-p/1555266#M1005</link>
      <description>&lt;P&gt;I am replacing the SE050 with A5000 on my schematic. The NXP documentation mentions the parts are pin-to-pin compatible.&lt;/P&gt;&lt;P&gt;However, the Pin Description table of the datasheets for the two parts differ when describing the RFU pins (originally used for ISO 7816 interface):&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;A5000 datasheet (Rev 1.2) recommends&lt;UL&gt;&lt;LI&gt;pin 3 and 13 to VCC&lt;/LI&gt;&lt;LI&gt;pin 14 to VSS&lt;/LI&gt;&lt;LI&gt;pin 16 to VIN&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;SE050 datasheet (Rev 3.7) recommends&lt;UL&gt;&lt;LI&gt;pin 3, 13, and 16 NC&lt;/LI&gt;&lt;LI&gt;pin 14 to VSS or VCC&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Which one is correct? Ideally I'd like to NC as many pins as possible to simplify layout routing.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Nov 2022 21:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A5000-RFU-pins-inconsistent-guidance-in-datasheet/m-p/1555266#M1005</guid>
      <dc:creator>michaelh2</dc:creator>
      <dc:date>2022-11-16T21:26:35Z</dc:date>
    </item>
    <item>
      <title>Re: A5000 RFU pins - inconsistent guidance in datasheet</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/A5000-RFU-pins-inconsistent-guidance-in-datasheet/m-p/1555552#M1007</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208893"&gt;@michaelh2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please following the&amp;nbsp;&lt;SPAN&gt;SE050 datasheet (Rev 3.7) recommendation, and the data sheet of A5000 will be updated accordingly in the future.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Sorry for the confusion that has caused.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 17 Nov 2022 06:42:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/A5000-RFU-pins-inconsistent-guidance-in-datasheet/m-p/1555552#M1007</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-11-17T06:42:40Z</dc:date>
    </item>
  </channel>
</rss>