<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K3 Functional Safety Mechanism Consultation in SafeAssure-Community</title>
    <link>https://community.nxp.com/t5/SafeAssure-Community/S32K3-Functional-Safety-Mechanism-Consultation/m-p/1896197#M108</link>
    <description>&lt;P&gt;S32K3 is designed with a lot of functional safety mechanisms, but in the actual product, there may be limited related functions that cannot be used, for example:&lt;/P&gt;&lt;P&gt;1.the ECU only uses SPI0 and does not use other SPI controllers, so do other SPI controllers need to be checked for SAF at this time?&lt;/P&gt;&lt;P&gt;2.If I don't use a CAN controller, do I need to check the CAN controller?&lt;/P&gt;&lt;P&gt;3.If you do not perform safety checks on unused peripheral resources, will the functions of the used peripheral resources be affected?&lt;/P&gt;</description>
    <pubDate>Sat, 29 Jun 2024 07:38:25 GMT</pubDate>
    <dc:creator>Yongxingjia</dc:creator>
    <dc:date>2024-06-29T07:38:25Z</dc:date>
    <item>
      <title>S32K3 Functional Safety Mechanism Consultation</title>
      <link>https://community.nxp.com/t5/SafeAssure-Community/S32K3-Functional-Safety-Mechanism-Consultation/m-p/1896197#M108</link>
      <description>&lt;P&gt;S32K3 is designed with a lot of functional safety mechanisms, but in the actual product, there may be limited related functions that cannot be used, for example:&lt;/P&gt;&lt;P&gt;1.the ECU only uses SPI0 and does not use other SPI controllers, so do other SPI controllers need to be checked for SAF at this time?&lt;/P&gt;&lt;P&gt;2.If I don't use a CAN controller, do I need to check the CAN controller?&lt;/P&gt;&lt;P&gt;3.If you do not perform safety checks on unused peripheral resources, will the functions of the used peripheral resources be affected?&lt;/P&gt;</description>
      <pubDate>Sat, 29 Jun 2024 07:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/SafeAssure-Community/S32K3-Functional-Safety-Mechanism-Consultation/m-p/1896197#M108</guid>
      <dc:creator>Yongxingjia</dc:creator>
      <dc:date>2024-06-29T07:38:25Z</dc:date>
    </item>
  </channel>
</rss>